<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MKV56F1M0VLQ24 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV56F1M0VLQ24/m-p/646166#M39193</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I think that the KV56 and KV58 are&amp;nbsp; pin to pin compatible for corresponding package, the only difference is that KV56 does not have Ethernet module and only have 2 CAN modules, while the KV58 has one Ethernet and 3 CAN modules.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14612iD04AB404EB1D586A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Apr 2017 04:18:20 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2017-04-27T04:18:20Z</dc:date>
    <item>
      <title>MKV56F1M0VLQ24</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV56F1M0VLQ24/m-p/646165#M39192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;The MKV58F1M0VLQ24 and MKV56F1M0VLQ24,the two Chip compatible?If I dont need Ethernet,the MKV56F1M0VLQ24 can replace MKV58F1M0VLQ24?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2017 09:28:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV56F1M0VLQ24/m-p/646165#M39192</guid>
      <dc:creator>tangliyusky</dc:creator>
      <dc:date>2017-04-26T09:28:45Z</dc:date>
    </item>
    <item>
      <title>Re: MKV56F1M0VLQ24</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV56F1M0VLQ24/m-p/646166#M39193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I think that the KV56 and KV58 are&amp;nbsp; pin to pin compatible for corresponding package, the only difference is that KV56 does not have Ethernet module and only have 2 CAN modules, while the KV58 has one Ethernet and 3 CAN modules.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14612iD04AB404EB1D586A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Apr 2017 04:18:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV56F1M0VLQ24/m-p/646166#M39193</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-04-27T04:18:20Z</dc:date>
    </item>
  </channel>
</rss>