<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Is DDR required for K-70 LCDC?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-DDR-required-for-K-70-LCDC/m-p/645886#M39184</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, customer can place picture at Flexbus connected MRAM memory.&lt;/P&gt;&lt;P&gt;It need to initialize Flexbus module during the system initialization phase (sysinit() at &amp;lt;start.c&amp;gt; file).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Dec 2016 05:18:40 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2016-12-29T05:18:40Z</dc:date>
    <item>
      <title>Is DDR required for K-70 LCDC?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-DDR-required-for-K-70-LCDC/m-p/645885#M39183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello friends,&lt;/P&gt;&lt;P&gt;I am working with MK70FN1M0VMJ12 UC. I don't use &lt;STRONG&gt;TWR-K70-RGB LCD&lt;/STRONG&gt; module. I want to control a TFT with &lt;SPAN&gt;MK70FN1M0VMJ12&lt;/SPAN&gt;k without an external chip (SSD1963 or ILI.....) &amp;nbsp;and I am using &amp;nbsp;"eGUI". I tried to export an image with "eGUI" (size : 800x600, bit depth: 24, format : jpg)&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;const LWord Aeshnid-ovipositing-800x600_data[] // array size:480000, 1875KB&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px; margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But SRAM and LCD-RAM are as follows.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#define __EXTERNAL_MRAM_ROM_BASE 0xA0000000&lt;BR /&gt;#define __EXTERNAL_MRAM_ROM_SIZE 0x00000000&lt;BR /&gt;#define __EXTERNAL_MRAM_RAM_BASE 0xA0000000&lt;BR /&gt;#define __EXTERNAL_MRAM_RAM_SIZE 0x00080000&lt;BR /&gt;#define __EXTERNAL_DDR2_RAM_BASE 0x70000000&lt;BR /&gt;#define __EXTERNAL_DDR2_RAM_SIZE 0x08000000&lt;BR /&gt;#define __EXTERNAL_LCD_BASE 0xA0010000&lt;BR /&gt;#define __EXTERNAL_LCD_SIZE 0x0001FFFF//127KB&lt;BR /&gt;#define __EXTERNAL_LCD_DC_BASE 0xA0000000&lt;/P&gt;&lt;P&gt;#define __INTERNAL_SRAM_BASE 0x1FFF0000&lt;BR /&gt;#define __INTERNAL_SRAM_SIZE 0x00020000//128KB&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, Do I have to use DDR for LCDC? &amp;nbsp;or &amp;nbsp;Can I compress this image via "eGUI"?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mehmet Okşan&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337617"&gt;800_600_jpg.h.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337617"&gt;800_600_jpg.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Dec 2016 13:25:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-DDR-required-for-K-70-LCDC/m-p/645885#M39183</guid>
      <dc:creator>mehmetoksan</dc:creator>
      <dc:date>2016-12-27T13:25:04Z</dc:date>
    </item>
    <item>
      <title>Re: Is DDR required for K-70 LCDC?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-DDR-required-for-K-70-LCDC/m-p/645886#M39184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, customer can place picture at Flexbus connected MRAM memory.&lt;/P&gt;&lt;P&gt;It need to initialize Flexbus module during the system initialization phase (sysinit() at &amp;lt;start.c&amp;gt; file).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Dec 2016 05:18:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-DDR-required-for-K-70-LCDC/m-p/645886#M39184</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-12-29T05:18:40Z</dc:date>
    </item>
  </channel>
</rss>