<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 GPIO outputs affected by wdog?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-outputs-affected-by-wdog/m-p/645876#M39181</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For the &amp;nbsp;MK22FN512CBP12R I want to configure some gpios as outputs to control some external chips. My question is if a watchdog reset occurs will these gpios revert to inputs? If so, is there any way to prevent this from occurring, since reverting to inputs could affect the control and state of the external chips?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Sep 2016 16:56:53 GMT</pubDate>
    <dc:creator>gsosnow</dc:creator>
    <dc:date>2016-09-23T16:56:53Z</dc:date>
    <item>
      <title>GPIO outputs affected by wdog?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-outputs-affected-by-wdog/m-p/645876#M39181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For the &amp;nbsp;MK22FN512CBP12R I want to configure some gpios as outputs to control some external chips. My question is if a watchdog reset occurs will these gpios revert to inputs? If so, is there any way to prevent this from occurring, since reverting to inputs could affect the control and state of the external chips?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Sep 2016 16:56:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-outputs-affected-by-wdog/m-p/645876#M39181</guid>
      <dc:creator>gsosnow</dc:creator>
      <dc:date>2016-09-23T16:56:53Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO outputs affected by wdog?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-outputs-affected-by-wdog/m-p/645877#M39182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;George&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A watchdog reset causes the GPIOs to be set to their default states - most as inputs or default peripheral functions.&lt;/P&gt;&lt;P&gt;If you want the states to be held in a particular state when this happens you will need to use external pullup and pull-downs to control the required state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Sep 2016 20:18:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-outputs-affected-by-wdog/m-p/645877#M39182</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-09-23T20:18:22Z</dc:date>
    </item>
  </channel>
</rss>