<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MQX with Flexbus on Kinetis K70 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-with-Flexbus-on-Kinetis-K70/m-p/219007#M3907</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pedro, I am connecting the TWR-K70 board with the TWR-LCD board using the elevator connectors and communicating via FlexBus, not using the LCDC but communicating with the screen directly. This works and I am able to display graphics on the screen when using a bare board project. I only have problems when also using MQX. Thanks, Harry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Jan 2013 18:14:02 GMT</pubDate>
    <dc:creator>awesomeclaw</dc:creator>
    <dc:date>2013-01-09T18:14:02Z</dc:date>
    <item>
      <title>MQX with Flexbus on Kinetis K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-with-Flexbus-on-Kinetis-K70/m-p/219005#M3905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to use the FlexBus interface to communicate between a TWR-K70 module and a TWR-LCD module when using MQX 4.0. However, I've found that MQX is somehow interfering with this (i.e., the same communication code works with a bare board project but not in MQX). What does MQX use the Flexbus interface for on the K70 and is there some way of disabling this use so that the FlexBus can be used for a user application?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Edit] Formatting&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Dec 2012 16:00:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-with-Flexbus-on-Kinetis-K70/m-p/219005#M3905</guid>
      <dc:creator>awesomeclaw</dc:creator>
      <dc:date>2012-12-28T16:00:03Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with Flexbus on Kinetis K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-with-Flexbus-on-Kinetis-K70/m-p/219006#M3906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Harry, how are you trying to connect the Flexbus and the TWR-LCD? are you connecting the TWR-LCD module directly to the TWR-K70 board using the primary/secondary elevator connectors?.&lt;/P&gt;&lt;P&gt;Please be advised you cannot do so, the problem is TWR-K70F120M can only interconnect directly with TWR-LCD-RGB since the controller board uses the LCDC dedicated bus instead of the Flexbus, so if you want to use the TWR-LCD you have to manually connect the TWR-K70F120M Flexbus lines to the TWR-LCD module.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2013 17:08:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-with-Flexbus-on-Kinetis-K70/m-p/219006#M3906</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2013-01-09T17:08:07Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with Flexbus on Kinetis K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-with-Flexbus-on-Kinetis-K70/m-p/219007#M3907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pedro, I am connecting the TWR-K70 board with the TWR-LCD board using the elevator connectors and communicating via FlexBus, not using the LCDC but communicating with the screen directly. This works and I am able to display graphics on the screen when using a bare board project. I only have problems when also using MQX. Thanks, Harry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2013 18:14:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-with-Flexbus-on-Kinetis-K70/m-p/219007#M3907</guid>
      <dc:creator>awesomeclaw</dc:creator>
      <dc:date>2013-01-09T18:14:02Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with Flexbus on Kinetis K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-with-Flexbus-on-Kinetis-K70/m-p/219008#M3908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Harry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You should include the d4dlcdhw_mqx_fb file in your MQX project, and check if in MQX 4.0 BSP_EXTERNAL_LCD_DC, BSP_EXTERNAL_LCD_BASE, etc are defined.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2013 18:26:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-with-Flexbus-on-Kinetis-K70/m-p/219008#M3908</guid>
      <dc:creator>LuisCasado</dc:creator>
      <dc:date>2013-01-09T18:26:32Z</dc:date>
    </item>
  </channel>
</rss>