<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: TWR-LCD Using FlexBus from K70</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-LCD-Using-FlexBus-from-K70/m-p/218900#M3904</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Herry:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm also trying to use LCD via flexbus interface on the same kit(k70) but in bareboard project.&lt;/P&gt;&lt;P&gt;can you share some sample code of that. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ankur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Sep 2015 08:42:23 GMT</pubDate>
    <dc:creator>ankurchauhan</dc:creator>
    <dc:date>2015-09-03T08:42:23Z</dc:date>
    <item>
      <title>TWR-LCD Using FlexBus from K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-LCD-Using-FlexBus-from-K70/m-p/218899#M3903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I'm trying to get the TWR-LCD module working via FlexBus from a TWR-K70F120M. I can get the screen to display content over SPI just fine, but I can't get any output when using the FlexBus interface. I read that there are problems with the IR circuitry interfering with FlexBus (www.utasker.com/docs/.../uTaskerV1.4_Kinetis_demo.pdf - page 10) and that the solution is to either remove some components from the board or cut a trace. Is this the case? Thanks!&lt;/P&gt;&lt;P&gt;[EDIT] OK, I neglected to mention that I was using an MQX project. It seems that when using the same Flexbus/LCD code on a bareboard project the LCD works correctly. Presumably then there is some problem with using Flexbus with MQX. I'll open a new question/discussion for that.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Dec 2012 15:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-LCD-Using-FlexBus-from-K70/m-p/218899#M3903</guid>
      <dc:creator>awesomeclaw</dc:creator>
      <dc:date>2012-12-28T15:20:04Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-LCD Using FlexBus from K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-LCD-Using-FlexBus-from-K70/m-p/218900#M3904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Herry:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm also trying to use LCD via flexbus interface on the same kit(k70) but in bareboard project.&lt;/P&gt;&lt;P&gt;can you share some sample code of that. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ankur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 08:42:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-LCD-Using-FlexBus-from-K70/m-p/218900#M3904</guid>
      <dc:creator>ankurchauhan</dc:creator>
      <dc:date>2015-09-03T08:42:23Z</dc:date>
    </item>
  </channel>
</rss>