<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K22 controller pin(TXD and RXD uart pins) operated on 5V (external device working on 5V supply)? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-controller-pin-TXD-and-RXD-uart-pins-operated-on-5V-external/m-p/643418#M39017</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on UART communication module of MK22FX512VMC12 controller. K22 controller operated on 3.3V supply and external communication module operated on 5V supply.my communication is working properly with external module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As per datasheet gpio pins operated on 5V &amp;nbsp;but no idea about uart communication module operating pin voltage 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it ok if i connect K22 controller UART pins(Txd, Rxd) to 5V operated module(Txd ,Rxd pins) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14643i912703659090B25B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/Sharad/tg-p"&gt;#Sharad&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Apr 2017 14:46:07 GMT</pubDate>
    <dc:creator>sharadpatil</dc:creator>
    <dc:date>2017-04-25T14:46:07Z</dc:date>
    <item>
      <title>K22 controller pin(TXD and RXD uart pins) operated on 5V (external device working on 5V supply)?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-controller-pin-TXD-and-RXD-uart-pins-operated-on-5V-external/m-p/643418#M39017</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on UART communication module of MK22FX512VMC12 controller. K22 controller operated on 3.3V supply and external communication module operated on 5V supply.my communication is working properly with external module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As per datasheet gpio pins operated on 5V &amp;nbsp;but no idea about uart communication module operating pin voltage 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it ok if i connect K22 controller UART pins(Txd, Rxd) to 5V operated module(Txd ,Rxd pins) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14643i912703659090B25B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/Sharad/tg-p"&gt;#Sharad&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Apr 2017 14:46:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-controller-pin-TXD-and-RXD-uart-pins-operated-on-5V-external/m-p/643418#M39017</guid>
      <dc:creator>sharadpatil</dc:creator>
      <dc:date>2017-04-25T14:46:07Z</dc:date>
    </item>
    <item>
      <title>Re: K22 controller pin(TXD and RXD uart pins) operated on 5V (external device working on 5V supply)?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-controller-pin-TXD-and-RXD-uart-pins-operated-on-5V-external/m-p/643419#M39018</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sharad,&lt;/P&gt;&lt;P&gt;The Kinetis Port pins are only 5V tolerant as inputs.&amp;nbsp; The outputs are not 5V tolerant, and that includes pins configured as open-drain outputs(Don't pullup to 5V).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Output pins(TXD) would only be driven to 3.3V. If the 5V device will recognize that as a high, then it's ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Apr 2017 02:19:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-controller-pin-TXD-and-RXD-uart-pins-operated-on-5V-external/m-p/643419#M39018</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-04-28T02:19:23Z</dc:date>
    </item>
  </channel>
</rss>