<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KW30Z minimal connection requirements in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW30Z-minimal-connection-requirements/m-p/642727#M38951</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Roman,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was checking your design and i have a few questions about your connections.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-The PTA2 is the reset for the SWD but you don't have to connect directly to the 3.3v, you can use a resistor for pull up.&lt;BR /&gt;-Are you are using a crystal oscilator?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I recommended to you see FRDM-KW40Z Freescale Freedom Development Board User's Guide for more details and a better reference.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/assets/documents/data/en/user-guides/FRDMKW40ZUG.pdf" title="http://www.nxp.com/assets/documents/data/en/user-guides/FRDMKW40ZUG.pdf"&gt;http://www.nxp.com/assets/documents/data/en/user-guides/FRDMKW40ZUG.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Dec 2016 18:19:32 GMT</pubDate>
    <dc:creator>mario_castaneda</dc:creator>
    <dc:date>2016-12-06T18:19:32Z</dc:date>
    <item>
      <title>KW30Z minimal connection requirements</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW30Z-minimal-connection-requirements/m-p/642726#M38950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have KW30Z chip soldered to qfn32 board and I'm trying to build simple protoboard to make basics tests. The problem is that I can't connect to the target chip with my CMSIS-DAP and J-Link adapters. I have read datasheet of KW30Z and schematics of FRDM-KW40Z(that should be almost the same chip) but still no luck. I see that DC-DC converter works, since I receive 1.8V and 1.5V on power output pins when I assemble buck layout. Also some other chips from ST work with same power lines connection(Only VDD, GND, NRST and SWD pins are connected, crystalless), So I think that Kinetis chips should work this way also. I attach my basic schematic with DC-DC in bypass &lt;SPAN&gt;layout&amp;nbsp;&lt;/SPAN&gt;that I suggest should work but it doesn't.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help is appreciated. Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="schematic.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8898i2E8179ED7FAEFA3A/image-size/large?v=v2&amp;amp;px=999" role="button" title="schematic.jpg" alt="schematic.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Dec 2016 20:07:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW30Z-minimal-connection-requirements/m-p/642726#M38950</guid>
      <dc:creator>romeoordos</dc:creator>
      <dc:date>2016-12-01T20:07:52Z</dc:date>
    </item>
    <item>
      <title>Re: KW30Z minimal connection requirements</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW30Z-minimal-connection-requirements/m-p/642727#M38951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Roman,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was checking your design and i have a few questions about your connections.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-The PTA2 is the reset for the SWD but you don't have to connect directly to the 3.3v, you can use a resistor for pull up.&lt;BR /&gt;-Are you are using a crystal oscilator?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I recommended to you see FRDM-KW40Z Freescale Freedom Development Board User's Guide for more details and a better reference.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/assets/documents/data/en/user-guides/FRDMKW40ZUG.pdf" title="http://www.nxp.com/assets/documents/data/en/user-guides/FRDMKW40ZUG.pdf"&gt;http://www.nxp.com/assets/documents/data/en/user-guides/FRDMKW40ZUG.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Dec 2016 18:19:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW30Z-minimal-connection-requirements/m-p/642727#M38951</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2016-12-06T18:19:32Z</dc:date>
    </item>
    <item>
      <title>Re: KW30Z minimal connection requirements</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW30Z-minimal-connection-requirements/m-p/642728#M38952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mario.&lt;/P&gt;&lt;P&gt;Thank you for response. I have resoldrered the chip and added pull-up resistor to PTA2. I have added decoupling capacitor to that pin also.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And now my j-link can connect and program it. So seems that issue is solved now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 10:10:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW30Z-minimal-connection-requirements/m-p/642728#M38952</guid>
      <dc:creator>romeoordos</dc:creator>
      <dc:date>2016-12-15T10:10:46Z</dc:date>
    </item>
  </channel>
</rss>