<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to generate Bootable code in FLASH using CW10.1 and Processor Expert? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-generate-Bootable-code-in-FLASH-using-CW10-1-and/m-p/218647#M3889</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I'm using the K60 part and have a project created in CW10.1 using Processor Expert.&amp;nbsp; I can&lt;/P&gt;&lt;P&gt;load and execute the program from internal RAM.&amp;nbsp; Whwn I change the debugger to&lt;/P&gt;&lt;P&gt;use the internal FLASH version, the code still loads into RAM, 0x1FFFXXXX.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I get CW to generate code that will load into the FLASH?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Jun 2011 10:48:56 GMT</pubDate>
    <dc:creator>FirmEE</dc:creator>
    <dc:date>2011-06-30T10:48:56Z</dc:date>
    <item>
      <title>How to generate Bootable code in FLASH using CW10.1 and Processor Expert?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-generate-Bootable-code-in-FLASH-using-CW10-1-and/m-p/218647#M3889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I'm using the K60 part and have a project created in CW10.1 using Processor Expert.&amp;nbsp; I can&lt;/P&gt;&lt;P&gt;load and execute the program from internal RAM.&amp;nbsp; Whwn I change the debugger to&lt;/P&gt;&lt;P&gt;use the internal FLASH version, the code still loads into RAM, 0x1FFFXXXX.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I get CW to generate code that will load into the FLASH?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jun 2011 10:48:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-generate-Bootable-code-in-FLASH-using-CW10-1-and/m-p/218647#M3889</guid>
      <dc:creator>FirmEE</dc:creator>
      <dc:date>2011-06-30T10:48:56Z</dc:date>
    </item>
    <item>
      <title>Re: How to generate Bootable code in FLASH using CW10.1 and Processor Expert?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-generate-Bootable-code-in-FLASH-using-CW10-1-and/m-p/218648#M3890</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For changing debug type of code memory to Flash it is necessary to change "Configurations" in project (of INTERNAL_RAM to INTERNAL_FLASH).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Steps for changing the configurations:&lt;BR /&gt;&amp;nbsp; 1. Right click on "INTERNAL_FLASH"&amp;nbsp; in “Configuration” folder tree&amp;nbsp; in project.&lt;BR /&gt;&amp;nbsp; 2. In pop-up menu select the "Select configuration as active".&lt;BR /&gt;&amp;nbsp; 3. Right click on "ProcessorExpert.pe" folder tree in project&amp;nbsp;and in pop-up menu select "Build configurations" -&amp;gt; "Set active" -&amp;gt; "XXX_INTERNAL_FLASH". This action selects active CPU from available “CPUs” in project tree configured to run code from FLASH memory.&lt;BR /&gt;&amp;nbsp; 4. Generate Processor Expert code.&lt;BR /&gt;&amp;nbsp; 5. Build project (Click on "Project" in Eclipse menu -&amp;gt; click on "Build project").&lt;BR /&gt;&amp;nbsp; 6. Click on "Run" in eclipse menu and select "Debug Configurations…" -&amp;gt; In window click on "CodeWarrior Download" in tree -&amp;gt; select project configuration "XXXX_INTENAL_FLASH_YYYY" -&amp;gt; click on "Debug" button.&lt;BR /&gt;&amp;nbsp; 7. Now it’s possible to debug your code from FLASH memory.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Jiri Rezler&lt;BR /&gt;Processor Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jul 2011 14:29:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-generate-Bootable-code-in-FLASH-using-CW10-1-and/m-p/218648#M3890</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2011-07-01T14:29:31Z</dc:date>
    </item>
  </channel>
</rss>