<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: USB-KW24D512 system reset will cause USB CDC module reset as well</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-KW24D512-system-reset-will-cause-USB-CDC-module-reset-as/m-p/641802#M38874</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot for your confirmation. Never mind, I will investigate&amp;nbsp;one possible solution&amp;nbsp;from application layer to deal with this situation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Xiao&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Feb 2017 05:38:13 GMT</pubDate>
    <dc:creator>xiaoma</dc:creator>
    <dc:date>2017-02-22T05:38:13Z</dc:date>
    <item>
      <title>USB-KW24D512 system reset will cause USB CDC module reset as well</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-KW24D512-system-reset-will-cause-USB-CDC-module-reset-as/m-p/641800#M38872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using USB CDC Driver&amp;nbsp;of USB-KW24D512 Dongle as a virtual com port on Windows OS. I can use Putty to communicate with the USB Dongle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One requirement for me now is that when the MCU occurs a software&amp;nbsp;reset (for example, set the SYSRESETREQ bit), I would like not to reset USB CDC module. If so, I need to restart the putty to connect with the device again. This is doable for manual configuration, however, that would not be a good way for automation software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Therefore, is there a way to bypass the USB CDC module reset when a system reset occurs or is there a kind of Reset which only erases the RAM memory?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Feb 2017 06:20:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-KW24D512-system-reset-will-cause-USB-CDC-module-reset-as/m-p/641800#M38872</guid>
      <dc:creator>xiaoma</dc:creator>
      <dc:date>2017-02-16T06:20:25Z</dc:date>
    </item>
    <item>
      <title>Re: USB-KW24D512 system reset will cause USB CDC module reset as well</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-KW24D512-system-reset-will-cause-USB-CDC-module-reset-as/m-p/641801#M38873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiao&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately USB FS module from the KW24 is a main module and there is not possible reset that could keep this module on. All resets will cause your USB mdoule to also reset. Sorry for the inconveniences that this may cause you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 04:45:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-KW24D512-system-reset-will-cause-USB-CDC-module-reset-as/m-p/641801#M38873</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-02-22T04:45:25Z</dc:date>
    </item>
    <item>
      <title>Re: USB-KW24D512 system reset will cause USB CDC module reset as well</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-KW24D512-system-reset-will-cause-USB-CDC-module-reset-as/m-p/641802#M38874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot for your confirmation. Never mind, I will investigate&amp;nbsp;one possible solution&amp;nbsp;from application layer to deal with this situation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Xiao&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 05:38:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-KW24D512-system-reset-will-cause-USB-CDC-module-reset-as/m-p/641802#M38874</guid>
      <dc:creator>xiaoma</dc:creator>
      <dc:date>2017-02-22T05:38:13Z</dc:date>
    </item>
  </channel>
</rss>