<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Swap disabling for the MK11DN512 device in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Swap-disabling-for-the-MK11DN512-device/m-p/641357#M38859</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're using the&amp;nbsp;MK11DN512 device.&lt;/P&gt;&lt;P&gt;Successfully used the swap mechanism to update firmware in the field a couple of times.&lt;/P&gt;&lt;P&gt;Now our firmware is about to grow above the half FLASH size, so we'd like to disable the swap, and use a "conventional" bootloader to update the FLASH.&lt;/P&gt;&lt;P&gt;From the swap document, it seems to be impossible to disable it.&lt;/P&gt;&lt;P&gt;Keeping the swap active, makes&amp;nbsp;a hole sector in the middle of the FLASH (for the swap indicator). This is mostly inconvenient.&lt;/P&gt;&lt;P&gt;We would like to disable it, without using the mass erase option, since it's a FOTA procedure, without development intervention.&lt;/P&gt;&lt;P&gt;We tried to erase those indicators, but the seems to be HW protected.&lt;/P&gt;&lt;P&gt;Is there any possibility to do it? maybe some sort of backdoor, or an undocumented&amp;nbsp;feature?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Isak.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 02 Apr 2017 06:37:09 GMT</pubDate>
    <dc:creator>isaklevinson</dc:creator>
    <dc:date>2017-04-02T06:37:09Z</dc:date>
    <item>
      <title>Swap disabling for the MK11DN512 device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Swap-disabling-for-the-MK11DN512-device/m-p/641357#M38859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're using the&amp;nbsp;MK11DN512 device.&lt;/P&gt;&lt;P&gt;Successfully used the swap mechanism to update firmware in the field a couple of times.&lt;/P&gt;&lt;P&gt;Now our firmware is about to grow above the half FLASH size, so we'd like to disable the swap, and use a "conventional" bootloader to update the FLASH.&lt;/P&gt;&lt;P&gt;From the swap document, it seems to be impossible to disable it.&lt;/P&gt;&lt;P&gt;Keeping the swap active, makes&amp;nbsp;a hole sector in the middle of the FLASH (for the swap indicator). This is mostly inconvenient.&lt;/P&gt;&lt;P&gt;We would like to disable it, without using the mass erase option, since it's a FOTA procedure, without development intervention.&lt;/P&gt;&lt;P&gt;We tried to erase those indicators, but the seems to be HW protected.&lt;/P&gt;&lt;P&gt;Is there any possibility to do it? maybe some sort of backdoor, or an undocumented&amp;nbsp;feature?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Isak.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Apr 2017 06:37:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Swap-disabling-for-the-MK11DN512-device/m-p/641357#M38859</guid>
      <dc:creator>isaklevinson</dc:creator>
      <dc:date>2017-04-02T06:37:09Z</dc:date>
    </item>
    <item>
      <title>Re: Swap disabling for the MK11DN512 device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Swap-disabling-for-the-MK11DN512-device/m-p/641358#M38860</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Isak,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I find below thread for your reference:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/379517"&gt;https://community.nxp.com/thread/379517&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Apr 2017 09:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Swap-disabling-for-the-MK11DN512-device/m-p/641358#M38860</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-04-06T09:33:56Z</dc:date>
    </item>
  </channel>
</rss>