<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Standalone Kinetis Flash Tools in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Standalone-Kinetis-Flash-Tools/m-p/641109#M38842</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;P&amp;amp;E's devices will do that. &amp;nbsp;I've got a Cyclone ACP on my desk at the moment, hooked up to a MK22FN1M0AVLH12, and the PROGACMP utility that came with it was able to read the flash contents just fine. &amp;nbsp;Should work with the Multilink, too. &amp;nbsp;Of course, this only works if security isn't enabled. &amp;nbsp;Here's a screen shot after using it to verify the loaded contents against the .elf file. &amp;nbsp;I was also able to download it to an .s19 file. &amp;nbsp;Not Intel HEX format, but a hex format, and easily converted to HEX or binary.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12465i72432805810CCC2B/image-size/large?v=v2&amp;amp;px=999" title="Screenshot 2017-01-28 18.55.20.png" alt="Screenshot 2017-01-28 18.55.20.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 29 Jan 2017 02:58:43 GMT</pubDate>
    <dc:creator>scottm</dc:creator>
    <dc:date>2017-01-29T02:58:43Z</dc:date>
    <item>
      <title>Standalone Kinetis Flash Tools</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Standalone-Kinetis-Flash-Tools/m-p/641108#M38841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm looking for standalone Kinetis Flash Tools which similar like FlashMagic on LPC &amp;nbsp;that can write/read the flash memory on Kinetis MCU.&lt;/P&gt;&lt;P&gt;The main function I need is to read out the whole flash memory as an Hex file to verify the memory crash issue.&lt;/P&gt;&lt;P&gt;Checked Cyclone and Multilink, it seems don't support this feature.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jan 2017 07:02:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Standalone-Kinetis-Flash-Tools/m-p/641108#M38841</guid>
      <dc:creator>yinyang</dc:creator>
      <dc:date>2017-01-25T07:02:46Z</dc:date>
    </item>
    <item>
      <title>Re: Standalone Kinetis Flash Tools</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Standalone-Kinetis-Flash-Tools/m-p/641109#M38842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;P&amp;amp;E's devices will do that. &amp;nbsp;I've got a Cyclone ACP on my desk at the moment, hooked up to a MK22FN1M0AVLH12, and the PROGACMP utility that came with it was able to read the flash contents just fine. &amp;nbsp;Should work with the Multilink, too. &amp;nbsp;Of course, this only works if security isn't enabled. &amp;nbsp;Here's a screen shot after using it to verify the loaded contents against the .elf file. &amp;nbsp;I was also able to download it to an .s19 file. &amp;nbsp;Not Intel HEX format, but a hex format, and easily converted to HEX or binary.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12465i72432805810CCC2B/image-size/large?v=v2&amp;amp;px=999" title="Screenshot 2017-01-28 18.55.20.png" alt="Screenshot 2017-01-28 18.55.20.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 29 Jan 2017 02:58:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Standalone-Kinetis-Flash-Tools/m-p/641109#M38842</guid>
      <dc:creator>scottm</dc:creator>
      <dc:date>2017-01-29T02:58:43Z</dc:date>
    </item>
    <item>
      <title>Re: Standalone Kinetis Flash Tools</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Standalone-Kinetis-Flash-Tools/m-p/641110#M38843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;USBDM provides utilities to read and write Kinetis devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Note you can only read unsecured devices&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a look at:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://usbdm.sourceforge.net/USBDM_V4.12/html/index.html" title="http://usbdm.sourceforge.net/USBDM_V4.12/html/index.html"&gt;USBDM: USBDM Debugger interface for Freescale RS08,HCS08,HCS12,Coldfire and ARM-Kinetis Devices.&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://usbdm.sourceforge.net/USBDM_V4.12/USBDM_JS16/html/index.html" title="http://usbdm.sourceforge.net/USBDM_V4.12/USBDM_JS16/html/index.html"&gt;USBDM: USBDM RS08/HCS08/HCS12/Coldfire V1,2,3,4/DSC/Kinetis Debugger and Programmer&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Programmers are available from several sources or you can build you own or recycle a FRDM board.&lt;/P&gt;&lt;P&gt;If buying one make sure it has a SWD interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Disclaimer: I wrote the above software/hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12507i1F4D4DC52DCED366/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12551iC419EAB9B7BC5004/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 29 Jan 2017 10:29:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Standalone-Kinetis-Flash-Tools/m-p/641110#M38843</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2017-01-29T10:29:49Z</dc:date>
    </item>
  </channel>
</rss>