<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: max external SDRAM size on K66F ?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/max-external-SDRAM-size-on-K66F/m-p/641075#M38836</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="291363" data-username="pwalh" href="https://community.nxp.com/people/pwalh"&gt;Pierre Walhin&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;The K66 can't support the SDRAM whose size beyond the 16 Mb.&lt;/P&gt;&lt;P&gt;Hope this is clear.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Dec 2016 06:18:00 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-12-05T06:18:00Z</dc:date>
    <item>
      <title>max external SDRAM size on K66F ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/max-external-SDRAM-size-on-K66F/m-p/641074#M38835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my company developed a device based on LPC1788. It features a two-chips 128MB SDRAM. The device is already in production.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are starting a new project in which we want to develop a new device with cloud connectivity. In this project, security is critical. Thus we are planning to use a Kinetis K66F which supports hardware encryption.&lt;/P&gt;&lt;P&gt;We also need at least 256MB SDRAM. 512MB would be best.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the K66 Ref Manual,&amp;nbsp;section 35.5.1, it is said that "The maximum SDRAM address size is 128 Mbits".&amp;nbsp;Does it mean that the maximum memory size is 16MB ? Or perhaps is it 16MB per chip select ? Is it at all possible to interface high capacity (512MB) SDRAM with a K66F ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance for your help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Dec 2016 13:49:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/max-external-SDRAM-size-on-K66F/m-p/641074#M38835</guid>
      <dc:creator>pwalh</dc:creator>
      <dc:date>2016-12-01T13:49:39Z</dc:date>
    </item>
    <item>
      <title>Re: max external SDRAM size on K66F ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/max-external-SDRAM-size-on-K66F/m-p/641075#M38836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="291363" data-username="pwalh" href="https://community.nxp.com/people/pwalh"&gt;Pierre Walhin&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;The K66 can't support the SDRAM whose size beyond the 16 Mb.&lt;/P&gt;&lt;P&gt;Hope this is clear.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Dec 2016 06:18:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/max-external-SDRAM-size-on-K66F/m-p/641075#M38836</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-12-05T06:18:00Z</dc:date>
    </item>
  </channel>
</rss>