<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TRK-KEA128 only communicating one way in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TRK-KEA128-only-communicating-one-way/m-p/640984#M38820</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have two microcontollers programmed such that when you press a button on one, it will send a message to the other to turn on a light. The message is sent via an interrupt on the button, but the communication only works one way. As in, if I set them both up to run, I can press the buttons on MCU 1 to turn on the lights on the MCU 2, but when I press the button on MCU 2, the light will not turn on on MCU 1. In fact, whichever MCU I press the button on first after running will work until I press a button on the other MCU, then the communication no longer works in either direction.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="175105_175105.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/122779i107556749749B94C/image-size/large?v=v2&amp;amp;px=999" role="button" title="175105_175105.png" alt="175105_175105.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12281i2950D192B10E5F9D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have a breakpoint set shortly after the MCU receives the message, and it will always stop at this breakpoint after pressing a button on the other MCU... but once I press a button on the receiving MCU, neither MCU will break after a button is pressed. I don't know if there is possibly a problem with the initial hardware setup before my code runs, but does anyone have an idea of why the message can only be distributed one direction?&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My project is attached below:&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Tyler&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Jan 2017 20:46:35 GMT</pubDate>
    <dc:creator>tylertrigg</dc:creator>
    <dc:date>2017-01-24T20:46:35Z</dc:date>
    <item>
      <title>TRK-KEA128 only communicating one way</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TRK-KEA128-only-communicating-one-way/m-p/640984#M38820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have two microcontollers programmed such that when you press a button on one, it will send a message to the other to turn on a light. The message is sent via an interrupt on the button, but the communication only works one way. As in, if I set them both up to run, I can press the buttons on MCU 1 to turn on the lights on the MCU 2, but when I press the button on MCU 2, the light will not turn on on MCU 1. In fact, whichever MCU I press the button on first after running will work until I press a button on the other MCU, then the communication no longer works in either direction.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="175105_175105.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/122779i107556749749B94C/image-size/large?v=v2&amp;amp;px=999" role="button" title="175105_175105.png" alt="175105_175105.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12281i2950D192B10E5F9D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have a breakpoint set shortly after the MCU receives the message, and it will always stop at this breakpoint after pressing a button on the other MCU... but once I press a button on the receiving MCU, neither MCU will break after a button is pressed. I don't know if there is possibly a problem with the initial hardware setup before my code runs, but does anyone have an idea of why the message can only be distributed one direction?&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My project is attached below:&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Tyler&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jan 2017 20:46:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TRK-KEA128-only-communicating-one-way/m-p/640984#M38820</guid>
      <dc:creator>tylertrigg</dc:creator>
      <dc:date>2017-01-24T20:46:35Z</dc:date>
    </item>
    <item>
      <title>Re: TRK-KEA128 only communicating one way</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TRK-KEA128-only-communicating-one-way/m-p/640985#M38821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First of all, sorry for the later reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had tested your code with two TRK-KEA128 board without any problem.&lt;/P&gt;&lt;P&gt;Please check attached video for the detailed info.&lt;/P&gt;&lt;P&gt;Below is TRK-KEA128 CAN PHY schematics, please check the STB_CAN pin voltage (it must be in low voltage, otherwise the CAN communication couldn't work)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13919iC52BD23BF1AD05B2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Feb 2017 06:25:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TRK-KEA128-only-communicating-one-way/m-p/640985#M38821</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-02-09T06:25:25Z</dc:date>
    </item>
  </channel>
</rss>