<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 LCD 5V with 1/8 cycles problem</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LCD-5V-with-1-8-cycles-problem/m-p/640842#M38812</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;I am using the K30 to drive my LCD. My LCD operate at 5V with 8x24 LCD 1/3 bias.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am able to run my LCD correctly after for few minutes. The problem comes after that. Some of the&amp;nbsp;segment&lt;/P&gt;&lt;P&gt;that is should be off is turn on. I realize that the segment affected is only those at the BP5-BP8.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Fyi, I am using charge pump to drive my LCD.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any register that I &amp;nbsp;need to define &amp;nbsp;beside LCD_GCR[DUTY] to make my LCD run properly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Dec 2016 06:04:47 GMT</pubDate>
    <dc:creator>blurblur</dc:creator>
    <dc:date>2016-12-01T06:04:47Z</dc:date>
    <item>
      <title>LCD 5V with 1/8 cycles problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LCD-5V-with-1-8-cycles-problem/m-p/640842#M38812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;I am using the K30 to drive my LCD. My LCD operate at 5V with 8x24 LCD 1/3 bias.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am able to run my LCD correctly after for few minutes. The problem comes after that. Some of the&amp;nbsp;segment&lt;/P&gt;&lt;P&gt;that is should be off is turn on. I realize that the segment affected is only those at the BP5-BP8.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Fyi, I am using charge pump to drive my LCD.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any register that I &amp;nbsp;need to define &amp;nbsp;beside LCD_GCR[DUTY] to make my LCD run properly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Dec 2016 06:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LCD-5V-with-1-8-cycles-problem/m-p/640842#M38812</guid>
      <dc:creator>blurblur</dc:creator>
      <dc:date>2016-12-01T06:04:47Z</dc:date>
    </item>
  </channel>
</rss>