<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MK64 default output at reset in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64-default-output-at-reset/m-p/640296#M38774</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the default state of the outputs of the cobtroller immidiately after reset?&lt;/P&gt;&lt;P&gt;Do i need to put pull up/pull down on board?Regarding inputs, do i need to place pull up/pull down on inputs (or outputs) not used?&lt;/P&gt;&lt;P&gt;I've looked in the data sheet but probabely missed it.&lt;/P&gt;&lt;P&gt;Any help will do.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Jan 2017 12:41:38 GMT</pubDate>
    <dc:creator>roymessinger</dc:creator>
    <dc:date>2017-01-24T12:41:38Z</dc:date>
    <item>
      <title>MK64 default output at reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64-default-output-at-reset/m-p/640296#M38774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the default state of the outputs of the cobtroller immidiately after reset?&lt;/P&gt;&lt;P&gt;Do i need to put pull up/pull down on board?Regarding inputs, do i need to place pull up/pull down on inputs (or outputs) not used?&lt;/P&gt;&lt;P&gt;I've looked in the data sheet but probabely missed it.&lt;/P&gt;&lt;P&gt;Any help will do.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jan 2017 12:41:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64-default-output-at-reset/m-p/640296#M38774</guid>
      <dc:creator>roymessinger</dc:creator>
      <dc:date>2017-01-24T12:41:38Z</dc:date>
    </item>
    <item>
      <title>Re: MK64 default output at reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64-default-output-at-reset/m-p/640297#M38775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The 'reset state' of all control registers is called out in the Reference Manual, including the 'pin mux' table, but the general statement is: 'reset state is the safest possible for any possible interconnect'.&amp;nbsp; That is, analog-in-capable pins will default to said analog-in mode, and digital pins will default to input, most with 'no pull'.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So yes, by-and-large anything you need to have as a 'known state' during/just-after reset will need your own external pull-resistors.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jan 2017 17:41:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64-default-output-at-reset/m-p/640297#M38775</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2017-01-24T17:41:31Z</dc:date>
    </item>
    <item>
      <title>Re: MK64 default output at reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64-default-output-at-reset/m-p/640298#M38776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Roy,&lt;/P&gt;&lt;P&gt;Some special function pins need take care. For exmaple: Reset_b\ NMI_b\ VREF_OUT\ JTAG_TMS&lt;/P&gt;&lt;P&gt;I recommend you read the "Chapter 2 General System Setup (Hardware Considerations)" of &lt;A href="http://www.nxp.com/assets/documents/data/en/quick-start-guide/KQRUG.pdf"&gt;KQRUG&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12366i53DEFEC599909CBA/image-size/large?v=v2&amp;amp;px=999" title="General System Setup (Hardware Considerations).png" alt="General System Setup (Hardware Considerations).png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jan 2017 00:28:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64-default-output-at-reset/m-p/640298#M38776</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-01-25T00:28:00Z</dc:date>
    </item>
  </channel>
</rss>