<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Firmware MK70</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Firmware-MK70/m-p/639038#M38618</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;I am using TWR K70 with external ddr2 ram.&lt;BR /&gt;I could put my firmware in a serial flash, and then copy it into RAM?&lt;BR /&gt;Is there any example?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you very much&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maurizio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Sep 2016 06:25:10 GMT</pubDate>
    <dc:creator>Microfelix</dc:creator>
    <dc:date>2016-09-22T06:25:10Z</dc:date>
    <item>
      <title>Firmware MK70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Firmware-MK70/m-p/639036#M38616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;I ask if it is possible on a K70 processor, you can use the firmware via an external FLASH.&lt;BR /&gt;The Indoor 1 Mbyte space is almost finished. If I need more space as I do?&lt;/P&gt;&lt;P&gt;Maurizio Felicioni&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 12:56:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Firmware-MK70/m-p/639036#M38616</guid>
      <dc:creator>Microfelix</dc:creator>
      <dc:date>2016-09-21T12:56:12Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware MK70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Firmware-MK70/m-p/639037#M38617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If your external Flash is parallel and memory mapped on the FlexBus it can be used for program code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Often external SDRAM is also used (faster) to run code from, after copying it there for a cheaper serial Flash, or NAND flash device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 21:40:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Firmware-MK70/m-p/639037#M38617</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-09-21T21:40:01Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware MK70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Firmware-MK70/m-p/639038#M38618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;I am using TWR K70 with external ddr2 ram.&lt;BR /&gt;I could put my firmware in a serial flash, and then copy it into RAM?&lt;BR /&gt;Is there any example?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you very much&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maurizio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 06:25:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Firmware-MK70/m-p/639038#M38618</guid>
      <dc:creator>Microfelix</dc:creator>
      <dc:date>2016-09-22T06:25:10Z</dc:date>
    </item>
  </channel>
</rss>