<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB Vregin input - MK64 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Vregin-input-MK64/m-p/638971#M38608</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Roy,&lt;/P&gt;&lt;P&gt;Connect VREGIN and VOUT33 together and tie to ground through a 10kΩ resistor.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12541iE9CC3B95CCBE05E2/image-size/large?v=v2&amp;amp;px=999" title="Unused analog interfaces.png" alt="Unused analog interfaces.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Jan 2017 01:55:29 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2017-01-24T01:55:29Z</dc:date>
    <item>
      <title>USB Vregin input - MK64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Vregin-input-MK64/m-p/638970#M38607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm designing a board based on the MK64 (the FRDM K64 is my reference design). I do not use the USB features of the MK64. I am using the UART capabilities (using USB dongle to RS485 cable from a far host PC to my controller board, then to UART inputs on the MK64 via a MAX3362 RS 485 Transceiver).&lt;/P&gt;&lt;P&gt;In such case, do I need to connect a voltage to that pin?&lt;/P&gt;&lt;P&gt;Leave it float?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jan 2017 16:33:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Vregin-input-MK64/m-p/638970#M38607</guid>
      <dc:creator>roymessinger</dc:creator>
      <dc:date>2017-01-23T16:33:46Z</dc:date>
    </item>
    <item>
      <title>Re: USB Vregin input - MK64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Vregin-input-MK64/m-p/638971#M38608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Roy,&lt;/P&gt;&lt;P&gt;Connect VREGIN and VOUT33 together and tie to ground through a 10kΩ resistor.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12541iE9CC3B95CCBE05E2/image-size/large?v=v2&amp;amp;px=999" title="Unused analog interfaces.png" alt="Unused analog interfaces.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jan 2017 01:55:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Vregin-input-MK64/m-p/638971#M38608</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-01-24T01:55:29Z</dc:date>
    </item>
    <item>
      <title>Re: USB Vregin input - MK64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Vregin-input-MK64/m-p/638972#M38609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok.&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P&gt;I've posted another question regarding un used I/O's and output state at reset.&lt;/P&gt;&lt;P&gt;Can you amswer that also?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jan 2017 12:17:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Vregin-input-MK64/m-p/638972#M38609</guid>
      <dc:creator>roymessinger</dc:creator>
      <dc:date>2017-01-24T12:17:25Z</dc:date>
    </item>
  </channel>
</rss>