<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KV5x RMII</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5x-RMII/m-p/637060#M38470</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RMII clock source can be EXTAL clock or ENET_1588_CLKIN selected via SIM_SOPT2[RMIISRC] selection.&lt;/P&gt;&lt;P&gt;So, the EXTAL pin or ENET_1588_CLKIN pin instead of RMII_REF_CLK pin's function.&lt;/P&gt;&lt;P&gt;Customer need consider to use EXTAL pin or ENET_1588_CLKIN pin.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/211iC360649A6437424B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Dec 2016 04:08:09 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2016-12-23T04:08:09Z</dc:date>
    <item>
      <title>KV5x RMII</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5x-RMII/m-p/637059#M38469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I'm try to design RMII mode network with MKV58F1M0VLQ24,but i can't find RMII_REF_CLK Pin in datasheet.Can you tell me ,which pin is RMII_REF_CLK?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Dec 2016 09:43:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5x-RMII/m-p/637059#M38469</guid>
      <dc:creator>tangliyusky</dc:creator>
      <dc:date>2016-12-22T09:43:07Z</dc:date>
    </item>
    <item>
      <title>Re: KV5x RMII</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5x-RMII/m-p/637060#M38470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RMII clock source can be EXTAL clock or ENET_1588_CLKIN selected via SIM_SOPT2[RMIISRC] selection.&lt;/P&gt;&lt;P&gt;So, the EXTAL pin or ENET_1588_CLKIN pin instead of RMII_REF_CLK pin's function.&lt;/P&gt;&lt;P&gt;Customer need consider to use EXTAL pin or ENET_1588_CLKIN pin.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/211iC360649A6437424B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Dec 2016 04:08:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5x-RMII/m-p/637060#M38470</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-12-23T04:08:09Z</dc:date>
    </item>
  </channel>
</rss>