<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using eDMA K22 to transfer data to a TFT LCD in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637054#M38464</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Use the BitBand macros in your processor header.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Probably like these:&lt;/P&gt;&lt;P&gt;/**&lt;BR /&gt;&amp;nbsp;* @brief Macro to calculate address of an aliased word in the peripheral&lt;BR /&gt;&amp;nbsp;*&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bitband area for a peripheral register and bit (bit band region 0x40000000 to&lt;BR /&gt;&amp;nbsp;*&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x400FFFFF).&lt;BR /&gt;&amp;nbsp;* @param Reg Register to access.&lt;BR /&gt;&amp;nbsp;* @param Bit Bit number to access.&lt;BR /&gt;&amp;nbsp;* @return&amp;nbsp; Address of the aliased word in the peripheral bitband area.&lt;BR /&gt;&amp;nbsp;*/&lt;BR /&gt;#define BITBAND_REGADDR(Reg,Bit) (0x42000000u + (32u*((uint32_t)&amp;amp;(Reg) - (uint32_t)0x40000000u)) + (4u*((uint32_t)(Bit))))&lt;BR /&gt;/**&lt;BR /&gt;&amp;nbsp;* @brief Macro to access a single bit of a peripheral register (bit band region&lt;BR /&gt;&amp;nbsp;*&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x40000000 to 0x400FFFFF) using the bit-band alias region access. Can&lt;BR /&gt;&amp;nbsp;*&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; be used for peripherals with 32bit access allowed.&lt;BR /&gt;&amp;nbsp;* @param Reg Register to access.&lt;BR /&gt;&amp;nbsp;* @param Bit Bit number to access.&lt;BR /&gt;&amp;nbsp;* @return Value of the targeted bit in the bit band region.&lt;BR /&gt;&amp;nbsp;*/&lt;BR /&gt;#define BITBAND_REG32(Reg,Bit) (*((uint32_t volatile*)(BITBAND_REGADDR(Reg,Bit))))&lt;BR /&gt;#define BITBAND_REG(Reg,Bit) (BITBAND_REG32(Reg,Bit))&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Apr 2017 15:45:31 GMT</pubDate>
    <dc:creator>egoodii</dc:creator>
    <dc:date>2017-04-18T15:45:31Z</dc:date>
    <item>
      <title>Using eDMA K22 to transfer data to a TFT LCD</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637051#M38461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have a device where i have MK22FX connected to a sdcard with the SDHC periferical and a LCD TFT. I have to read the data image from the sdcard and write this to the LCD that is interfaced with a 8bit parallel port. Every byte write to the TFT need to be validate with a rising edge of a GPIO of write. My question is if it is possible program the eDMA to control also this pin so all the data transfer is done only with the eDMA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is my first time that i want to use this periferical.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2017 07:48:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637051#M38461</guid>
      <dc:creator>danielecortella</dc:creator>
      <dc:date>2017-02-15T07:48:25Z</dc:date>
    </item>
    <item>
      <title>Re: Using eDMA K22 to transfer data to a TFT LCD</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637052#M38462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniele,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a bit-band region allowing user to access the GPIO module, so you may use eDMA to transfer data to this space to control the GPIO pin rise or fall. Please kindly refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14616i06AA4B4829B15D0C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope that helps,&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Feb 2017 04:25:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637052#M38462</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2017-02-17T04:25:30Z</dc:date>
    </item>
    <item>
      <title>Re: Using eDMA K22 to transfer data to a TFT LCD</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637053#M38463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;on my kinetis datasheet is written that the bitband GPIO controller address is&amp;nbsp;0x400F_F000. So my question is, if i want to write a 1 to the GPIOC0 how i have to calculate the address where to write?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Apr 2017 18:38:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637053#M38463</guid>
      <dc:creator>danielecortella</dc:creator>
      <dc:date>2017-04-17T18:38:03Z</dc:date>
    </item>
    <item>
      <title>Re: Using eDMA K22 to transfer data to a TFT LCD</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637054#M38464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Use the BitBand macros in your processor header.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Probably like these:&lt;/P&gt;&lt;P&gt;/**&lt;BR /&gt;&amp;nbsp;* @brief Macro to calculate address of an aliased word in the peripheral&lt;BR /&gt;&amp;nbsp;*&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bitband area for a peripheral register and bit (bit band region 0x40000000 to&lt;BR /&gt;&amp;nbsp;*&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x400FFFFF).&lt;BR /&gt;&amp;nbsp;* @param Reg Register to access.&lt;BR /&gt;&amp;nbsp;* @param Bit Bit number to access.&lt;BR /&gt;&amp;nbsp;* @return&amp;nbsp; Address of the aliased word in the peripheral bitband area.&lt;BR /&gt;&amp;nbsp;*/&lt;BR /&gt;#define BITBAND_REGADDR(Reg,Bit) (0x42000000u + (32u*((uint32_t)&amp;amp;(Reg) - (uint32_t)0x40000000u)) + (4u*((uint32_t)(Bit))))&lt;BR /&gt;/**&lt;BR /&gt;&amp;nbsp;* @brief Macro to access a single bit of a peripheral register (bit band region&lt;BR /&gt;&amp;nbsp;*&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x40000000 to 0x400FFFFF) using the bit-band alias region access. Can&lt;BR /&gt;&amp;nbsp;*&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; be used for peripherals with 32bit access allowed.&lt;BR /&gt;&amp;nbsp;* @param Reg Register to access.&lt;BR /&gt;&amp;nbsp;* @param Bit Bit number to access.&lt;BR /&gt;&amp;nbsp;* @return Value of the targeted bit in the bit band region.&lt;BR /&gt;&amp;nbsp;*/&lt;BR /&gt;#define BITBAND_REG32(Reg,Bit) (*((uint32_t volatile*)(BITBAND_REGADDR(Reg,Bit))))&lt;BR /&gt;#define BITBAND_REG(Reg,Bit) (BITBAND_REG32(Reg,Bit))&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Apr 2017 15:45:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637054#M38464</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2017-04-18T15:45:31Z</dc:date>
    </item>
    <item>
      <title>Re: Using eDMA K22 to transfer data to a TFT LCD</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637055#M38465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for the reply. So if i want to write high the GPIOD PIN2 for example i have to set:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reg Register =&amp;nbsp;GPIOD_PDOR is 400F_F0C0h base&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Bit Bit = 2&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;so i have the bitband address, writing 1 on this i will set the bit:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;*(calcuate_address) = 0x1U&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;right?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Apr 2017 06:08:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637055#M38465</guid>
      <dc:creator>danielecortella</dc:creator>
      <dc:date>2017-04-19T06:08:27Z</dc:date>
    </item>
    <item>
      <title>Re: Using eDMA K22 to transfer data to a TFT LCD</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637056#M38466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The LSB is indeed what interacts with the bit-banding hardware.&amp;nbsp; So yes, to 'set' your bit:&lt;/P&gt;&lt;P&gt;BITBAND_REG(GPIOD_PDOR, 2) = 1;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A particular place where 'bit band' hardware and macro come in VERY handy is to test a Boolean flag bit in a register, and especially for 'write 1 clear' w1c bits in such registers for 'interrupt acknowledge' without RMW or disturbing anything else!&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;STRONG&gt; if( BITBAND_REG(I2S0_RCSR, I2S_RCSR_FEF_SHIFT) )&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x10ee4: 0xf8df 0x1ae0&amp;nbsp; LDR.W&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; R1, [PC, #0xae0]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; [0x119c8] 0x425e1048 (1113460808)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x10ee8: 0x6809&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LDR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; R1, [R1]&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x10eea: 0xb119&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CBZ&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; R1, ??I2S0_RX_IRQHandler_3 ; 0x10ef4&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;STRONG&gt;BITBAND_REG(I2S0_RCSR, I2S_RCSR_FEF_SHIFT) = 1;&lt;/STRONG&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x10eec: 0xf8df 0x1ad8&amp;nbsp; LDR.W&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; R1, [PC, #0xad8]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; [0x119c8] 0x425e1048 (1113460808)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x10ef0: 0x2201&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MOVS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; R2, #1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x10ef2: 0x600a&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; STR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; R2, [R1]&lt;/P&gt;&lt;P&gt;??I2S0_RX_IRQHandler_3:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Apr 2017 11:45:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637056#M38466</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2017-04-19T11:45:58Z</dc:date>
    </item>
    <item>
      <title>Re: Using eDMA K22 to transfer data to a TFT LCD</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637057#M38467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;with my new pcb i'm trying this solution but i have a problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have to set the pin of LCD_WR high and then low&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;BR /&gt; GPIO_WritePinOutput(LCD_WR_GPIO_BASE, LCD_WR_GPIO_PIN, false);//write low&lt;BR /&gt; tmp = GPIOC-&amp;gt;PDOR &amp;amp; 0xFFFFFF00;&lt;BR /&gt; GPIOC-&amp;gt;PDOR = tmp | data;&lt;BR /&gt; GPIO_WritePinOutput(LCD_WR_GPIO_BASE, LCD_WR_GPIO_PIN, true);//write high&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;so i have modified the function as&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;BR /&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;BITBAND_REG&lt;/SPAN&gt;(&lt;SPAN style="background-color: #f6f6f6;"&gt;GPIOB-&amp;gt;PDOR&lt;/SPAN&gt;, LCD_WR_GPIO_PIN) = 1;//write low&lt;BR /&gt; tmp = GPIOC-&amp;gt;PDOR &amp;amp; 0xFFFFFF00;&lt;BR /&gt; GPIOC-&amp;gt;PDOR = tmp | data;&lt;BR /&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;BITBAND_REG&lt;/SPAN&gt;(&lt;SPAN style="background-color: #f6f6f6;"&gt;GPIOB-&amp;gt;PDOR&lt;/SPAN&gt;, LCD_WR_GPIO_PIN) = 0;//write high&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;where&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;LCD_WR_GPIO_PIN &amp;nbsp; &amp;nbsp; 21U&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;BITBAND_REGADDR function in defined in the MK22 file as:&lt;/SPAN&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;/**&lt;BR /&gt; * @brief Macro to calculate address of an aliased word in the peripheral&lt;BR /&gt; * bitband area for a peripheral register and bit (bit band region 0x40000000 to&lt;BR /&gt; * 0x400FFFFF).&lt;BR /&gt; * @param Reg Register to access.&lt;BR /&gt; * @param Bit Bit number to access.&lt;BR /&gt; * @return Address of the aliased word in the peripheral bitband area.&lt;BR /&gt; */&lt;BR /&gt;#define BITBAND_REGADDR(Reg,Bit) (0x42000000u + (32u*((uint32_t)&amp;amp;(Reg) - (uint32_t)0x40000000u)) + (4u*((uint32_t)(Bit))))&lt;BR /&gt;/**&lt;BR /&gt; * @brief Macro to access a single bit of a peripheral register (bit band region&lt;BR /&gt; * 0x40000000 to 0x400FFFFF) using the bit-band alias region access. Can&lt;BR /&gt; * be used for peripherals with 32bit access allowed.&lt;BR /&gt; * @param Reg Register to access.&lt;BR /&gt; * @param Bit Bit number to access.&lt;BR /&gt; * @return Value of the targeted bit in the bit band region.&lt;BR /&gt; */&lt;BR /&gt;#define BITBAND_REG32(Reg,Bit) (*((uint32_t volatile*)(BITBAND_REGADDR((Reg),(Bit)))))&lt;BR /&gt;#define BITBAND_REG(Reg,Bit) (BITBAND_REG32((Reg),(Bit)))&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;but the code dosn't work. Can you help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jul 2017 07:53:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637057#M38467</guid>
      <dc:creator>danielecortella</dc:creator>
      <dc:date>2017-07-12T07:53:43Z</dc:date>
    </item>
    <item>
      <title>Re: Using eDMA K22 to transfer data to a TFT LCD</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637058#M38468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;up&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jul 2017 09:31:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-eDMA-K22-to-transfer-data-to-a-TFT-LCD/m-p/637058#M38468</guid>
      <dc:creator>danielecortella</dc:creator>
      <dc:date>2017-07-18T09:31:58Z</dc:date>
    </item>
  </channel>
</rss>