<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Output File Format from CW 10.1</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Output-File-Format-from-CW-10-1/m-p/217483#M3845</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was wondering about the differences between a .afx file and .S19 file that's created as a result of a Codewarrior 10.1 project build. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the project properties window under the C/C++ Build node, the Settings option containts a Build Artifacts tab that lists the output file extension that defaults to afx. &amp;nbsp;Is this an ARM ELF format? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There's also an option in the Tool Settings tab, under ARM Linker-&amp;gt;Output, to generate an S-Record File. &amp;nbsp;Is the data contained in the .S19 sufficient to program the firmware into the K60 flash? &amp;nbsp;If I were to buy a JTAG programmer to program chips on a production board, would I need to load the .S19 file or the .afx file?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Jun 2011 22:50:59 GMT</pubDate>
    <dc:creator>TravisHidlay</dc:creator>
    <dc:date>2011-06-24T22:50:59Z</dc:date>
    <item>
      <title>Output File Format from CW 10.1</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Output-File-Format-from-CW-10-1/m-p/217483#M3845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was wondering about the differences between a .afx file and .S19 file that's created as a result of a Codewarrior 10.1 project build. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the project properties window under the C/C++ Build node, the Settings option containts a Build Artifacts tab that lists the output file extension that defaults to afx. &amp;nbsp;Is this an ARM ELF format? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There's also an option in the Tool Settings tab, under ARM Linker-&amp;gt;Output, to generate an S-Record File. &amp;nbsp;Is the data contained in the .S19 sufficient to program the firmware into the K60 flash? &amp;nbsp;If I were to buy a JTAG programmer to program chips on a production board, would I need to load the .S19 file or the .afx file?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jun 2011 22:50:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Output-File-Format-from-CW-10-1/m-p/217483#M3845</guid>
      <dc:creator>TravisHidlay</dc:creator>
      <dc:date>2011-06-24T22:50:59Z</dc:date>
    </item>
    <item>
      <title>Re: Output File Format from CW 10.1</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Output-File-Format-from-CW-10-1/m-p/217484#M3846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;S19 is just a binary&amp;nbsp;data (with addresses) -&amp;nbsp;it is text format with hex numbers inside.&lt;/P&gt;&lt;P&gt;AXF is binary and includes the code and all symbols.&lt;/P&gt;&lt;P&gt;Most programmers take binary and hex files, so it is enough for flashing, but not full-blown debugging.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We do offer production-level (batch-mode) flashing of Kinetis parts (including OTP and locking options).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BTW (this is an answer to your other post) - our JTAGjet emulator can be used to debug production level boards.&lt;/P&gt;&lt;P&gt;We also support ETM trace for Kinetis parts.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please take a look into &lt;A href="http://www.signum.com/freescale.htm" rel="nofollow" target="_blank"&gt;www.signum.com/freescale.htm&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Jun 2011 04:33:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Output-File-Format-from-CW-10-1/m-p/217484#M3846</guid>
      <dc:creator>RobertSignum</dc:creator>
      <dc:date>2011-06-25T04:33:04Z</dc:date>
    </item>
  </channel>
</rss>