<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Remotely Upgrading Firmware?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Remotely-Upgrading-Firmware/m-p/217321#M3837</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See the following: &lt;A href="http://www.utasker.com/docs/uTasker/uTaskerBoot_003.PDF%FEFF" rel="nofollow" target="_self"&gt;http://www.utasker.com/docs/uTasker/uTaskerBoot_003.PDF﻿&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This works also on the Kinetis and allows Ethernet (including encrypted) firmware uploading via Ethernet (typically FTP or HTTP from a web browser).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It involves installing a boot loader (varying in size from about 2k to about 20k if a standalone web server based loader is required.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If local firmware uploads are required also serial and USB can be used - see &lt;A href="http://www.youtube.com/watch?v=H4TYM9jY2-g%FEFF" rel="nofollow" target="_self"&gt;http://www.youtube.com/watch?v=H4TYM9jY2-g﻿&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't think that there are any advantages of switching Flash blocks as part of the loader sequence.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Jun 2011 04:50:59 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2011-06-24T04:50:59Z</dc:date>
    <item>
      <title>Remotely Upgrading Firmware?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Remotely-Upgrading-Firmware/m-p/217320#M3836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a general question about whether or not it's possible to remotely install brand new firmware on a Kinetis micro.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The processor would be programmed for use in a product before shipping, but I'd like to be able to add the possibility of remotely reprogramming it over a network, using just the kinetis as the processor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas on how this could be accomplished in the K60? &amp;nbsp;I noticed a section on page 104 of the K60P144 Reference Manual that mentions a feature for swapping the starting address of the program flash blocks between block 0 and block 1. &amp;nbsp;Would it be possible to store a new binary to block 1 or 0 and switch the starting address, then reboot into the new firmware?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jun 2011 00:51:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Remotely-Upgrading-Firmware/m-p/217320#M3836</guid>
      <dc:creator>TravisHidlay</dc:creator>
      <dc:date>2011-06-24T00:51:42Z</dc:date>
    </item>
    <item>
      <title>Re: Remotely Upgrading Firmware?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Remotely-Upgrading-Firmware/m-p/217321#M3837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See the following: &lt;A href="http://www.utasker.com/docs/uTasker/uTaskerBoot_003.PDF%FEFF" rel="nofollow" target="_self"&gt;http://www.utasker.com/docs/uTasker/uTaskerBoot_003.PDF﻿&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This works also on the Kinetis and allows Ethernet (including encrypted) firmware uploading via Ethernet (typically FTP or HTTP from a web browser).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It involves installing a boot loader (varying in size from about 2k to about 20k if a standalone web server based loader is required.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If local firmware uploads are required also serial and USB can be used - see &lt;A href="http://www.youtube.com/watch?v=H4TYM9jY2-g%FEFF" rel="nofollow" target="_self"&gt;http://www.youtube.com/watch?v=H4TYM9jY2-g﻿&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't think that there are any advantages of switching Flash blocks as part of the loader sequence.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jun 2011 04:50:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Remotely-Upgrading-Firmware/m-p/217321#M3837</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2011-06-24T04:50:59Z</dc:date>
    </item>
    <item>
      <title>Re: Remotely Upgrading Firmware?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Remotely-Upgrading-Firmware/m-p/217322#M3838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Mark, I'll take a look at this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jun 2011 21:51:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Remotely-Upgrading-Firmware/m-p/217322#M3838</guid>
      <dc:creator>TravisHidlay</dc:creator>
      <dc:date>2011-06-24T21:51:43Z</dc:date>
    </item>
  </channel>
</rss>