<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Freedom K64F: starting without debugger?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-K64F-starting-without-debugger/m-p/634778#M38272</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, on the FRDM-K64F the rest line has this already. That comment was a general one in case a custom board is used.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Dec 2016 06:56:17 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2016-12-23T06:56:17Z</dc:date>
    <item>
      <title>Freedom K64F: starting without debugger?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-K64F-starting-without-debugger/m-p/634775#M38269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an application running on Freedom K64F (using Segger JLink, SDK2.1). &lt;BR /&gt;Application is stored in flash and runs absolutely fine under debugger.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like the board to run the application when powered up without the debugger - but nothing happens. &lt;BR /&gt;I disabled EZport per Erich's blog &lt;A href="https://mcuoneclipse.com/"&gt;https://mcuoneclipse.com/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6i84E40910DF05A8DD/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Traces are cut to onboard debugger as detailed here: &lt;A href="https://developer.mbed.org/questions/4658/FRDM-K64F-alternative-JTAG-Debugger/"&gt;https://developer.mbed.org/questions/4658/FRDM-K64F-alternative-JTAG-Debugger/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So what am I missing?&lt;BR /&gt;Thanks!&lt;BR /&gt;Best Regards, Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Dec 2016 14:36:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-K64F-starting-without-debugger/m-p/634775#M38269</guid>
      <dc:creator>davenadler</dc:creator>
      <dc:date>2016-12-22T14:36:37Z</dc:date>
    </item>
    <item>
      <title>Re: Freedom K64F: starting without debugger?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-K64F-starting-without-debugger/m-p/634776#M38270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would have a look at the RESET and NMI lines (is NMI disabled?).&lt;/P&gt;&lt;P&gt;The Reset line should have a pull-up (say 10k) with a capacitor (say 1uF).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Dec 2016 19:50:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-K64F-starting-without-debugger/m-p/634776#M38270</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-12-22T19:50:23Z</dc:date>
    </item>
    <item>
      <title>Re: Freedom K64F: starting without debugger?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-K64F-starting-without-debugger/m-p/634777#M38271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I disabled NMI in FOPT as well, same behavior (hope I did this right):&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208i3B23C7BDEDEE3949/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Not sure I understand about the RESET line - I'm using the K64F Freedom board; shouldn't this be already set up?&lt;/P&gt;&lt;P&gt;Thanks Erich, Best Regards, Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Dec 2016 21:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-K64F-starting-without-debugger/m-p/634777#M38271</guid>
      <dc:creator>davenadler</dc:creator>
      <dc:date>2016-12-22T21:04:02Z</dc:date>
    </item>
    <item>
      <title>Re: Freedom K64F: starting without debugger?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-K64F-starting-without-debugger/m-p/634778#M38272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, on the FRDM-K64F the rest line has this already. That comment was a general one in case a custom board is used.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Dec 2016 06:56:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-K64F-starting-without-debugger/m-p/634778#M38272</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-12-23T06:56:17Z</dc:date>
    </item>
    <item>
      <title>Re: Freedom K64F: starting without debugger?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-K64F-starting-without-debugger/m-p/634779#M38273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;The problem was caused by semi-hosting. This project used &lt;SPAN style="font-size: small; font-family: Consolas,monospace;"&gt;-specs=rdimon.specs&lt;/SPAN&gt; to linker to support SWO output debug connection. The library support for SWO is too lame to notice no debugger attached, and hangs in the startup code awaiting a debugger connection prior entering main. Oddly, IIRC I used semi-hosting for a couple products I developed using NXP LPC11C14 and LPC Xpresso, and I don't recall seeing this problem before. Anyway, just adjust the linker options:&lt;BR /&gt;- Remove:&amp;nbsp; &lt;SPAN style="font-family: Consolas,monospace; font-size: 13px;"&gt;-specs=rdimon.specs&lt;/SPAN&gt;&lt;BR /&gt; - Add:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN style="font-family: Consolas,monospace; font-size: 13px;"&gt;-specs=nosys.specs&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Hope that helps someone else,&lt;BR /&gt;Best Regards, Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Dec 2016 13:35:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-K64F-starting-without-debugger/m-p/634779#M38273</guid>
      <dc:creator>davenadler</dc:creator>
      <dc:date>2016-12-27T13:35:05Z</dc:date>
    </item>
  </channel>
</rss>