<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: cpu running slowly after wake up from STOP mode in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634762#M38264</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tuomas aaltio,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; What the KL25 code you are using? KSDK2.0-FRDM-KL25?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I didn't find the KSDK for KL25 using SMC_PostExitStopModes, so you can comment it, when the interrupt happens, the code will exit stop mode. if SMC_PostExitStopModes is used for the clock mode switch, fore example, PBE to PEE, because just as I have said, PEE enter STOP, wakeup will be PBE, clock switch to PEE need time. If you you don't want to do this clock switch, you can use other clock mode to enter STOP, then you don't need to do the clock mode switch after waking up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Mar 2017 03:29:15 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2017-03-14T03:29:15Z</dc:date>
    <item>
      <title>cpu running slowly after wake up from STOP mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634756#M38258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What causes cpu to run slowly after wake up? Code puts cpu to STOP mode and wakeup is TMP isr. It works otherwise but the cpu is running slowly. When running code with out stop mode, isr takes 1us. With stop mode isr takes 12us.&lt;/P&gt;&lt;P&gt;frdm-kl25z board (KL25Z128VLK).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Mar 2017 08:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634756#M38258</guid>
      <dc:creator>tuomasaaltio</dc:creator>
      <dc:date>2017-03-08T08:55:36Z</dc:date>
    </item>
    <item>
      <title>Re: cpu running slowly after wake up from STOP mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634757#M38259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;code to enten stop mode:&lt;/P&gt;&lt;P&gt;&amp;nbsp;SMC_PreEnterStopModes();&lt;BR /&gt;&amp;nbsp;SMC_SetPowerModeStop(SMC, kSMC_PartialStop);&lt;BR /&gt;&amp;nbsp;SMC_PostExitStopModes();&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Mar 2017 10:11:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634757#M38259</guid>
      <dc:creator>tuomasaaltio</dc:creator>
      <dc:date>2017-03-08T10:11:09Z</dc:date>
    </item>
    <item>
      <title>Re: cpu running slowly after wake up from STOP mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634758#M38260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tuomas aaltio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Please check this picture at first:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/16238i9C54B79422DE2EC1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Take care, if you are using PEE mode, after exit the STOP, the clock mode is PBE, so your clock is changed, you need to change PBE to PEE again to keep the same clock frequency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 09:26:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634758#M38260</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-03-09T09:26:41Z</dc:date>
    </item>
    <item>
      <title>Re: cpu running slowly after wake up from STOP mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634759#M38261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;now code execution speed is ok, but it takes surprisingly long time to start, 80us. That is the time between TMP module interrupt trigger (can be seen from pwm signal and cpu current consumption)&amp;nbsp; to isr to run. Is wake-up from STOP mode really so slow?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 10:27:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634759#M38261</guid>
      <dc:creator>tuomasaaltio</dc:creator>
      <dc:date>2017-03-09T10:27:20Z</dc:date>
    </item>
    <item>
      <title>Re: cpu running slowly after wake up from STOP mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634760#M38262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tuomas aaltio,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; STOP to RUN wake up is normally 4us, but if you do the clock mode switch, then run the TPM again, the clock mode switch also need to cause time, but this time is not the wake up time.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/16736i544A189023B854C3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 10:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634760#M38262</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-03-09T10:43:06Z</dc:date>
    </item>
    <item>
      <title>Re: cpu running slowly after wake up from STOP mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634761#M38263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;reason for slow start is routine&lt;/P&gt;&lt;P&gt;SMC_PostExitStopModes();&lt;/P&gt;&lt;P&gt;that takes 100us. Is there way avoid using it? something I could use instead.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Mar 2017 14:25:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634761#M38263</guid>
      <dc:creator>tuomasaaltio</dc:creator>
      <dc:date>2017-03-13T14:25:47Z</dc:date>
    </item>
    <item>
      <title>Re: cpu running slowly after wake up from STOP mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634762#M38264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tuomas aaltio,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; What the KL25 code you are using? KSDK2.0-FRDM-KL25?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I didn't find the KSDK for KL25 using SMC_PostExitStopModes, so you can comment it, when the interrupt happens, the code will exit stop mode. if SMC_PostExitStopModes is used for the clock mode switch, fore example, PBE to PEE, because just as I have said, PEE enter STOP, wakeup will be PBE, clock switch to PEE need time. If you you don't want to do this clock switch, you can use other clock mode to enter STOP, then you don't need to do the clock mode switch after waking up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Mar 2017 03:29:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634762#M38264</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-03-14T03:29:15Z</dc:date>
    </item>
    <item>
      <title>Re: cpu running slowly after wake up from STOP mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634763#M38265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SDK_2.1_FRDM-KL25Z&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Mar 2017 06:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/cpu-running-slowly-after-wake-up-from-STOP-mode/m-p/634763#M38265</guid>
      <dc:creator>tuomasaaltio</dc:creator>
      <dc:date>2017-03-14T06:15:58Z</dc:date>
    </item>
  </channel>
</rss>