<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: getting started with MKL25Z64VFM4 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/getting-started-with-MKL25Z64VFM4/m-p/634305#M38217</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I recommend you read &lt;A href="http://www.nxp.com/assets/documents/data/en/user-guides/KLQRUG.pdf"&gt;Kinetis L Peripheral Module Quick Reference&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;This collection of code examples, useful tips, and quick reference material has been created to help you speed the development of your applications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See section "2.1.5.1 Debug interface":&lt;BR /&gt;The SWD_CLK pin has an internal pull down device and SWD_DIO has an internal pull up device. An external 4.7 kΩ to 10 kΩ pullup is recommended for the SWD_DIO pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See also "2.1.3.4.1 RESET_b and NMI_b":&lt;BR /&gt;The RESET_b pin, if enabled, should have a 100 nF capacitor close to the MCU for transient protection. The NMI_b pin, if enabled, must not have any capacitance connected to it. Each pin, when enabled as their default function, has a weak internal pullup, but an external 4.7 kΩ to 10 kΩ pullup is recommended.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;---------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Dec 2016 13:33:22 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2016-12-22T13:33:22Z</dc:date>
    <item>
      <title>getting started with MKL25Z64VFM4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/getting-started-with-MKL25Z64VFM4/m-p/634304#M38216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm using this uC for the first time. &amp;nbsp;I&amp;nbsp;want to use SWD however within all the documentation (see attached) I have reviewed, I have not found information indicating if I need pull-up resistors or not on the SWD_CLK, SWD_DIO lines. &amp;nbsp;Can someone advise me where I can find this information so I know where to look in the future.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Brian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Dec 2016 02:56:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/getting-started-with-MKL25Z64VFM4/m-p/634304#M38216</guid>
      <dc:creator>briancavanagh</dc:creator>
      <dc:date>2016-12-22T02:56:14Z</dc:date>
    </item>
    <item>
      <title>Re: getting started with MKL25Z64VFM4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/getting-started-with-MKL25Z64VFM4/m-p/634305#M38217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I recommend you read &lt;A href="http://www.nxp.com/assets/documents/data/en/user-guides/KLQRUG.pdf"&gt;Kinetis L Peripheral Module Quick Reference&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;This collection of code examples, useful tips, and quick reference material has been created to help you speed the development of your applications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See section "2.1.5.1 Debug interface":&lt;BR /&gt;The SWD_CLK pin has an internal pull down device and SWD_DIO has an internal pull up device. An external 4.7 kΩ to 10 kΩ pullup is recommended for the SWD_DIO pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See also "2.1.3.4.1 RESET_b and NMI_b":&lt;BR /&gt;The RESET_b pin, if enabled, should have a 100 nF capacitor close to the MCU for transient protection. The NMI_b pin, if enabled, must not have any capacitance connected to it. Each pin, when enabled as their default function, has a weak internal pullup, but an external 4.7 kΩ to 10 kΩ pullup is recommended.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;---------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Dec 2016 13:33:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/getting-started-with-MKL25Z64VFM4/m-p/634305#M38217</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2016-12-22T13:33:22Z</dc:date>
    </item>
  </channel>
</rss>