<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Design flow chart of secure application code.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Design-flow-chart-of-secure-application-code/m-p/633552#M38164</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to design my own application code that have 3 below features.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Can not read from flash without my secure key.&lt;/P&gt;&lt;P&gt;2) Can not write into flash without my private key.&lt;/P&gt;&lt;P&gt;3) My code can also able to flash the data into flash memory once i enter exact key. And during flashing no one can retrieve &amp;nbsp; &amp;nbsp; my data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SO i need a help to make flow chart and basic idea to make that possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MKE18F512VLL16. I want to send and receive the data via LPUART0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Apr 2017 22:12:03 GMT</pubDate>
    <dc:creator>rohitchudasama</dc:creator>
    <dc:date>2017-04-21T22:12:03Z</dc:date>
    <item>
      <title>Design flow chart of secure application code.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Design-flow-chart-of-secure-application-code/m-p/633552#M38164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to design my own application code that have 3 below features.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Can not read from flash without my secure key.&lt;/P&gt;&lt;P&gt;2) Can not write into flash without my private key.&lt;/P&gt;&lt;P&gt;3) My code can also able to flash the data into flash memory once i enter exact key. And during flashing no one can retrieve &amp;nbsp; &amp;nbsp; my data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SO i need a help to make flow chart and basic idea to make that possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MKE18F512VLL16. I want to send and receive the data via LPUART0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Apr 2017 22:12:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Design-flow-chart-of-secure-application-code/m-p/633552#M38164</guid>
      <dc:creator>rohitchudasama</dc:creator>
      <dc:date>2017-04-21T22:12:03Z</dc:date>
    </item>
    <item>
      <title>Re: Design flow chart of secure application code.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Design-flow-chart-of-secure-application-code/m-p/633553#M38165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a very useful application note AN4507 about Kinetis security and Flash protection feature.&lt;/P&gt;&lt;P&gt;More detailed info, please check &lt;A href="http://www.nxp.com/assets/documents/data/en/application-notes/AN4507.pdf"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact, when the Kinetis chip was secured. The JTAG/SWD debug port can not access the on-chip Flash.&lt;/P&gt;&lt;P&gt;Customer application code can access internal Flash whatever the Kinetis was secured or not.&lt;/P&gt;&lt;P&gt;So, customer can use UART module as an interface to receive the key to lock/unlock Kinetis.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 May 2017 09:01:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Design-flow-chart-of-secure-application-code/m-p/633553#M38165</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-05-10T09:01:39Z</dc:date>
    </item>
  </channel>
</rss>