<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: new usb class</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/new-usb-class/m-p/633132#M38134</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Julien Rochette&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;USBTMC is based with USB 2.0 Specification, so yes, you can implement it. Basically it's just following the USBTMC specifications and make sure you have the descriptors and USBTMC requests correctly implemented.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We don't provide with such a class in Kinetis USB stack, but it is possible, for further information please refer to &lt;A href="http://www.usb.org/developers/docs/devclass_docs/"&gt;USB Test &amp;amp; Measurements class specification &lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Feb 2017 04:52:31 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2017-02-24T04:52:31Z</dc:date>
    <item>
      <title>new usb class</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/new-usb-class/m-p/633131#M38133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, is it possible to create a new usb class not initially supported by the usb stack or does it have to be supported initially?&lt;BR /&gt;I'm using the K22F and want to create a USBTMC device.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Julien.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Feb 2017 20:06:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/new-usb-class/m-p/633131#M38133</guid>
      <dc:creator>julienrochette</dc:creator>
      <dc:date>2017-02-14T20:06:33Z</dc:date>
    </item>
    <item>
      <title>Re: new usb class</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/new-usb-class/m-p/633132#M38134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Julien Rochette&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;USBTMC is based with USB 2.0 Specification, so yes, you can implement it. Basically it's just following the USBTMC specifications and make sure you have the descriptors and USBTMC requests correctly implemented.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We don't provide with such a class in Kinetis USB stack, but it is possible, for further information please refer to &lt;A href="http://www.usb.org/developers/docs/devclass_docs/"&gt;USB Test &amp;amp; Measurements class specification &lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Feb 2017 04:52:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/new-usb-class/m-p/633132#M38134</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-02-24T04:52:31Z</dc:date>
    </item>
  </channel>
</rss>