<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: USB stack sample project TWR-K20D50M modification</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-stack-sample-project-TWR-K20D50M-modification/m-p/216909#M3813</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The USB operation requires a high resolution 48MHz clock (&amp;lt; 0.25% or 2'500ppm). Although it is possible to generate this from the 8MHz RC oscillator it will only be approximate and usually outside fo the USB tolerance specification, meaning that it either won't work or will work only unreliably.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Designs requiring USB therefore need an accurate clock source - usually a clock or a quarz (for the main oscillator or on the USB clock input - for chips with this option). The only exception is if the RC oscillator can be tuned to obtain an accurate enough clock but this will probably only be accurate at a stable temperature and so is only really an option for experimental work, such as a school project where only one device needs to work in a controlled environment. For anything that will go into production it would however be begging for big (technical and subsequnt financial) problems ;-)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Oct 2012 12:39:44 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2012-10-12T12:39:44Z</dc:date>
    <item>
      <title>USB stack sample project TWR-K20D50M modification</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-stack-sample-project-TWR-K20D50M-modification/m-p/216908#M3812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;what changes should I make in a Freescale USB stack sample project for TWR-K20D50M to be able to use it on my own board with MK20DX256 MCU. My board has 8 MHz RC resonator, USB connector connected directly to MK20DX256 and some other stuff. At the moment any of the USB stack sample project doesn't work - PC doesn't recognize usb device.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2012 07:12:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-stack-sample-project-TWR-K20D50M-modification/m-p/216908#M3812</guid>
      <dc:creator>gaminn</dc:creator>
      <dc:date>2012-10-12T07:12:18Z</dc:date>
    </item>
    <item>
      <title>Re: USB stack sample project TWR-K20D50M modification</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-stack-sample-project-TWR-K20D50M-modification/m-p/216909#M3813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The USB operation requires a high resolution 48MHz clock (&amp;lt; 0.25% or 2'500ppm). Although it is possible to generate this from the 8MHz RC oscillator it will only be approximate and usually outside fo the USB tolerance specification, meaning that it either won't work or will work only unreliably.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Designs requiring USB therefore need an accurate clock source - usually a clock or a quarz (for the main oscillator or on the USB clock input - for chips with this option). The only exception is if the RC oscillator can be tuned to obtain an accurate enough clock but this will probably only be accurate at a stable temperature and so is only really an option for experimental work, such as a school project where only one device needs to work in a controlled environment. For anything that will go into production it would however be begging for big (technical and subsequnt financial) problems ;-)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2012 12:39:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-stack-sample-project-TWR-K20D50M-modification/m-p/216909#M3813</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2012-10-12T12:39:44Z</dc:date>
    </item>
    <item>
      <title>Re: USB stack sample project TWR-K20D50M modification</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-stack-sample-project-TWR-K20D50M-modification/m-p/216910#M3814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Mark,&lt;/P&gt;&lt;P&gt;thank you for your hint about RC resonator. I will replace it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, the USB stack sample projects work for me now even with the resonator - it was software problem, I didn't edit the source code of the sample project properly so USB interrupt was not enabled. Stupid mistake...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2012 20:21:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-stack-sample-project-TWR-K20D50M-modification/m-p/216910#M3814</guid>
      <dc:creator>gaminn</dc:creator>
      <dc:date>2012-10-12T20:21:33Z</dc:date>
    </item>
  </channel>
</rss>