<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 TWR-KM34 and meter software examples</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-KM34-and-meter-software-examples/m-p/630852#M37966</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello support,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to compile the IAR demo software for the&amp;nbsp;Software-for-One-Phase-Power-Meter.zip&lt;/P&gt;&lt;P&gt;It was done in IAR 6.5 and I have IAR 7.60&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Their are several projects and i get the same error so I am missing something or missing a setting up procedure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\Freescale\KM128SWDRV_R3_0_0\build\iar_6_50\projects&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Readme file:&lt;/P&gt;&lt;P&gt;Kinetis M One-phase Power Meter Application 3.0.04.0 (November 11, 2014).&lt;/P&gt;&lt;P&gt;Applications installs together with KM128SWDRV_R3_0_0. Refer to AN4265.pdf and DRM143.pdf for more information about filter-based metering algorithm and Kinetis-M one phase power meter reference design. Performance of the metering algorithm can be tuned using filter-based metering algorithm configuration tool.&lt;/P&gt;&lt;P&gt;Release Notes: refer to mk341phX.c source files for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My IAR error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Error[Lp049]: there was no reference to __iar_data_init3, but it is needed to initialize section .bss (adc.o #8) &lt;BR /&gt;Error[Lp048]: the init table "Table" is needed to initialize some variables, but there are no references to it &lt;BR /&gt;Error while running Linker &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I get the same error when trying to comple the E-Meter demo for the TWR&lt;/P&gt;&lt;P&gt;C:\Freescale\KMSWDRV_EAR2_2\build\iar_6_50\projects\_twr_emeter_demo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please provide some guidance ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Mar 2017 17:40:39 GMT</pubDate>
    <dc:creator>dkh</dc:creator>
    <dc:date>2017-03-07T17:40:39Z</dc:date>
    <item>
      <title>TWR-KM34 and meter software examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-KM34-and-meter-software-examples/m-p/630852#M37966</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello support,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to compile the IAR demo software for the&amp;nbsp;Software-for-One-Phase-Power-Meter.zip&lt;/P&gt;&lt;P&gt;It was done in IAR 6.5 and I have IAR 7.60&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Their are several projects and i get the same error so I am missing something or missing a setting up procedure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\Freescale\KM128SWDRV_R3_0_0\build\iar_6_50\projects&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Readme file:&lt;/P&gt;&lt;P&gt;Kinetis M One-phase Power Meter Application 3.0.04.0 (November 11, 2014).&lt;/P&gt;&lt;P&gt;Applications installs together with KM128SWDRV_R3_0_0. Refer to AN4265.pdf and DRM143.pdf for more information about filter-based metering algorithm and Kinetis-M one phase power meter reference design. Performance of the metering algorithm can be tuned using filter-based metering algorithm configuration tool.&lt;/P&gt;&lt;P&gt;Release Notes: refer to mk341phX.c source files for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My IAR error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Error[Lp049]: there was no reference to __iar_data_init3, but it is needed to initialize section .bss (adc.o #8) &lt;BR /&gt;Error[Lp048]: the init table "Table" is needed to initialize some variables, but there are no references to it &lt;BR /&gt;Error while running Linker &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I get the same error when trying to comple the E-Meter demo for the TWR&lt;/P&gt;&lt;P&gt;C:\Freescale\KMSWDRV_EAR2_2\build\iar_6_50\projects\_twr_emeter_demo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please provide some guidance ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Mar 2017 17:40:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-KM34-and-meter-software-examples/m-p/630852#M37966</guid>
      <dc:creator>dkh</dc:creator>
      <dc:date>2017-03-07T17:40:39Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-KM34 and meter software examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-KM34-and-meter-software-examples/m-p/630853#M37967</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Answer can be found here;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/433565"&gt;https://community.nxp.com/thread/433565&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Mar 2017 19:06:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-KM34-and-meter-software-examples/m-p/630853#M37967</guid>
      <dc:creator>dkh</dc:creator>
      <dc:date>2017-03-07T19:06:49Z</dc:date>
    </item>
  </channel>
</rss>