<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Hello, is possible use Li-SOCl2 battery with open circuit voltage 3,68V to direct power MKL16Z128VFT4? It is only 80 mV over maximum voltage in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hello-is-possible-use-Li-SOCl2-battery-with-open-circuit-voltage/m-p/630540#M37928</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have low power device powered with pimary battery and we would like avoid to use voltage regulator because it has own consumption. Selected battery has over 3,6V (around 3,68V at 20°C in open circuit). What MCU for these conditions? Is it OK to use?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Nov 2016 11:58:42 GMT</pubDate>
    <dc:creator>tomasnez</dc:creator>
    <dc:date>2016-11-29T11:58:42Z</dc:date>
    <item>
      <title>Hello, is possible use Li-SOCl2 battery with open circuit voltage 3,68V to direct power MKL16Z128VFT4? It is only 80 mV over maximum voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hello-is-possible-use-Li-SOCl2-battery-with-open-circuit-voltage/m-p/630540#M37928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have low power device powered with pimary battery and we would like avoid to use voltage regulator because it has own consumption. Selected battery has over 3,6V (around 3,68V at 20°C in open circuit). What MCU for these conditions? Is it OK to use?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Nov 2016 11:58:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hello-is-possible-use-Li-SOCl2-battery-with-open-circuit-voltage/m-p/630540#M37928</guid>
      <dc:creator>tomasnez</dc:creator>
      <dc:date>2016-11-29T11:58:42Z</dc:date>
    </item>
    <item>
      <title>Re: Hello, is possible use Li-SOCl2 battery with open circuit voltage 3,68V to direct power MKL16Z128VFT4? It is only 80 mV over maximum voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hello-is-possible-use-Li-SOCl2-battery-with-open-circuit-voltage/m-p/630541#M37929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; From the MKL16Z128VF4 datasheet, we can get that the max data of VDD is 3.6 V.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; So we highly recommend the customer use the VDD is in the range of 1.71 to 3.6v, if the voltage is higher, it may cause the chip damaged.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; But from my own experience about the lithium battery, the open circuit voltage normally is higher than the closed circuit voltage, if you add the load, the battery voltage may lower than 3.6V. You can try to add your batter to the MKL16, and then test the vdd, whether it is in the range of 1.71 to 3.6V, if yes, you can use it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Nov 2016 05:07:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hello-is-possible-use-Li-SOCl2-battery-with-open-circuit-voltage/m-p/630541#M37929</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-11-30T05:07:11Z</dc:date>
    </item>
  </channel>
</rss>