<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MKL03Z8 unresponsive after entering vlls3 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03Z8-unresponsive-after-entering-vlls3/m-p/630436#M37926</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I have been tinkering with the MKL03Z8.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The IDE has been IAR with the TI MPS432 Launchpad, in cmsis-dap mode, and the STM32 Discovery Kit as debugger probes. Everything has been fine for a month or two with "countless" downloads and debugging sessions. Both debuggers worked good with the Launchpad having slightly better functionalty whereas the STM32 was a little faster at downloading. The application main structure is the kind where most time is spent sleeping (seconds) , then waking up briefly, take some ADC measurements, and then back to sleep. VLPR -&amp;gt; VLPS with LPTMR clocked by LPO as wake-up source. It all worked well and battery economy was good (4-6 uA).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was then testing &amp;nbsp;VLLS modes to see if battery economy could become even better and vlls3 did shave off another 1.5uA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problem was, that when I finished that debugger session, I could no longer connect to target.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Fatal Error: Failed to connect to CPU".&lt;/P&gt;&lt;P&gt;This is with the MSP432 Launchpad debugger. The STM32 Disco has an equivalent &amp;nbsp;message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Same problem in all debugger RESET modes: System, Software, Hardware.&lt;/P&gt;&lt;P&gt;The STM32 Disco has an extra RESET mode which looked promising (Connect Under Reset), but no luck.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All 5 HW connections between debugger probe(s) and target have been and are direct with no resistors or caps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;+3V, GROUND, RST, SWDIO, SWDCLK. From time to time I've had a 4.7uF cap between +3V and Ground.&lt;/P&gt;&lt;P&gt;(before the problem started I often had to disconnect RST in order for a download to happen. Dunno why, ignored it.)&lt;/P&gt;&lt;P&gt;Most of the time I've had the debugger(s) &amp;nbsp;"Leave target running".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Varying the SWD clock: all combinations tried, same result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mass erase: same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the code in the (unresponsive) target MKL03Z8:&amp;nbsp;&lt;/P&gt;&lt;P&gt;NV_FOPT = FTFA_FOPT &amp;nbsp;= 0x0A. So slow reset into VLPR,&amp;nbsp;NMI_b pin disabled, BOOTPIN_OPT=1 (flash boot).&lt;/P&gt;&lt;P&gt;NV_FOPT is the only NV_ byte that has been modified, so I guess there should not be an issue with flash security.&lt;/P&gt;&lt;P&gt;I am not sure if interrupts are on or off. Perhaps permanently off. Coming out of RESET (not POR) code may never set ACKISO or restore I/0 pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, does anybody know how I can connect the IDE and debugger to this target again?&lt;/P&gt;&lt;P&gt;Or, alternatively, forgetting this specific MKL03Z8, is there something I can do to make sure that I will always be able to recover from something like this? Like different NV_ byte(s), different FTFA_FOPT or something else?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help will be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Peter Kobl&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Mar 2017 17:56:55 GMT</pubDate>
    <dc:creator>PeterK</dc:creator>
    <dc:date>2017-03-07T17:56:55Z</dc:date>
    <item>
      <title>MKL03Z8 unresponsive after entering vlls3</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03Z8-unresponsive-after-entering-vlls3/m-p/630436#M37926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I have been tinkering with the MKL03Z8.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The IDE has been IAR with the TI MPS432 Launchpad, in cmsis-dap mode, and the STM32 Discovery Kit as debugger probes. Everything has been fine for a month or two with "countless" downloads and debugging sessions. Both debuggers worked good with the Launchpad having slightly better functionalty whereas the STM32 was a little faster at downloading. The application main structure is the kind where most time is spent sleeping (seconds) , then waking up briefly, take some ADC measurements, and then back to sleep. VLPR -&amp;gt; VLPS with LPTMR clocked by LPO as wake-up source. It all worked well and battery economy was good (4-6 uA).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was then testing &amp;nbsp;VLLS modes to see if battery economy could become even better and vlls3 did shave off another 1.5uA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problem was, that when I finished that debugger session, I could no longer connect to target.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Fatal Error: Failed to connect to CPU".&lt;/P&gt;&lt;P&gt;This is with the MSP432 Launchpad debugger. The STM32 Disco has an equivalent &amp;nbsp;message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Same problem in all debugger RESET modes: System, Software, Hardware.&lt;/P&gt;&lt;P&gt;The STM32 Disco has an extra RESET mode which looked promising (Connect Under Reset), but no luck.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All 5 HW connections between debugger probe(s) and target have been and are direct with no resistors or caps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;+3V, GROUND, RST, SWDIO, SWDCLK. From time to time I've had a 4.7uF cap between +3V and Ground.&lt;/P&gt;&lt;P&gt;(before the problem started I often had to disconnect RST in order for a download to happen. Dunno why, ignored it.)&lt;/P&gt;&lt;P&gt;Most of the time I've had the debugger(s) &amp;nbsp;"Leave target running".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Varying the SWD clock: all combinations tried, same result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mass erase: same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the code in the (unresponsive) target MKL03Z8:&amp;nbsp;&lt;/P&gt;&lt;P&gt;NV_FOPT = FTFA_FOPT &amp;nbsp;= 0x0A. So slow reset into VLPR,&amp;nbsp;NMI_b pin disabled, BOOTPIN_OPT=1 (flash boot).&lt;/P&gt;&lt;P&gt;NV_FOPT is the only NV_ byte that has been modified, so I guess there should not be an issue with flash security.&lt;/P&gt;&lt;P&gt;I am not sure if interrupts are on or off. Perhaps permanently off. Coming out of RESET (not POR) code may never set ACKISO or restore I/0 pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, does anybody know how I can connect the IDE and debugger to this target again?&lt;/P&gt;&lt;P&gt;Or, alternatively, forgetting this specific MKL03Z8, is there something I can do to make sure that I will always be able to recover from something like this? Like different NV_ byte(s), different FTFA_FOPT or something else?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help will be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Peter Kobl&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Mar 2017 17:56:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03Z8-unresponsive-after-entering-vlls3/m-p/630436#M37926</guid>
      <dc:creator>PeterK</dc:creator>
      <dc:date>2017-03-07T17:56:55Z</dc:date>
    </item>
    <item>
      <title>Re: MKL03Z8 unresponsive after entering vlls3</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03Z8-unresponsive-after-entering-vlls3/m-p/630437#M37927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found a way to do this&lt;/P&gt;&lt;P&gt;with inspiration from thread&amp;nbsp;&lt;A href="https://community.nxp.com/thread/445747"&gt;https://community.nxp.com/thread/445747&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Setup:&lt;/P&gt;&lt;P&gt;IAR IDE (EWARM),&lt;/P&gt;&lt;P&gt;MSP432 XDS110 Launchpad debugger in cmsis-dap mode. Option: CMSIS-DAP&amp;gt;Setup&amp;gt;Reset set to "Hardware",&lt;/P&gt;&lt;P&gt;5 wires straight from debugger to target (+3V, GND, SWDCLK, SWDRST, and SWDIO).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When failing the "Fatal error ,," message would pop up about 4 seconds "into" the download.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But with an extra wire connecting GND and SWDRST, and having initiated the download, and then pulling the wire out again after 2-3 seconds, the download continues and succeeds. Target could then be used in the usual ways.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hopefully this may be helpful to somebody else.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-- Peter Kobl&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Mar 2017 10:31:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03Z8-unresponsive-after-entering-vlls3/m-p/630437#M37927</guid>
      <dc:creator>PeterK</dc:creator>
      <dc:date>2017-03-08T10:31:50Z</dc:date>
    </item>
  </channel>
</rss>