<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Code execution from external Flash</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-execution-from-external-Flash/m-p/630297#M37917</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After the K22 product reset, the code execute from internal Flash.&lt;/P&gt;&lt;P&gt;While, customer still could jump to execute the code located in external Flash via FlexBus interface.&lt;/P&gt;&lt;P&gt;The FlexBus module could interface with external NOR Flash or MRAM products.&lt;/P&gt;&lt;P&gt;The K22 product should initialize the FlexBus module at first. After that, jump the application from internal Flash to external Flash.&lt;/P&gt;&lt;P&gt;The FlexBus clock is up to 50MHz, while it need take 4 cycles to read data(instruction)(not using burst mode) with related port size.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Apr 2017 05:19:07 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2017-04-05T05:19:07Z</dc:date>
    <item>
      <title>Code execution from external Flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-execution-from-external-Flash/m-p/630296#M37916</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to execute a code on kinetis K22 using external Flash ?&lt;/P&gt;&lt;P&gt;If so, what are the recommendations for flash type, interface type &amp;amp; execution performance ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;Eduard&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/amirshteinberg"&gt;amirshteinberg&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Mar 2017 07:49:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-execution-from-external-Flash/m-p/630296#M37916</guid>
      <dc:creator>razumovskyeduar</dc:creator>
      <dc:date>2017-03-29T07:49:00Z</dc:date>
    </item>
    <item>
      <title>Re: Code execution from external Flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-execution-from-external-Flash/m-p/630297#M37917</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After the K22 product reset, the code execute from internal Flash.&lt;/P&gt;&lt;P&gt;While, customer still could jump to execute the code located in external Flash via FlexBus interface.&lt;/P&gt;&lt;P&gt;The FlexBus module could interface with external NOR Flash or MRAM products.&lt;/P&gt;&lt;P&gt;The K22 product should initialize the FlexBus module at first. After that, jump the application from internal Flash to external Flash.&lt;/P&gt;&lt;P&gt;The FlexBus clock is up to 50MHz, while it need take 4 cycles to read data(instruction)(not using burst mode) with related port size.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Apr 2017 05:19:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-execution-from-external-Flash/m-p/630297#M37917</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-04-05T05:19:07Z</dc:date>
    </item>
  </channel>
</rss>