<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックCan K21 USBDCD use for detect VBUS status?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-K21-USBDCD-use-for-detect-VBUS-status/m-p/630144#M37911</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anybody tell me if K21&amp;nbsp;USBDCD can use for detect VBUS status? And how to do?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Jan 2017 10:08:37 GMT</pubDate>
    <dc:creator>jimyang</dc:creator>
    <dc:date>2017-01-20T10:08:37Z</dc:date>
    <item>
      <title>Can K21 USBDCD use for detect VBUS status?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-K21-USBDCD-use-for-detect-VBUS-status/m-p/630144#M37911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anybody tell me if K21&amp;nbsp;USBDCD can use for detect VBUS status? And how to do?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2017 10:08:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-K21-USBDCD-use-for-detect-VBUS-status/m-p/630144#M37911</guid>
      <dc:creator>jimyang</dc:creator>
      <dc:date>2017-01-20T10:08:37Z</dc:date>
    </item>
    <item>
      <title>Re: Can K21 USBDCD use for detect VBUS status?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-K21-USBDCD-use-for-detect-VBUS-status/m-p/630145#M37912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jim Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We recommend to use a GPIO pin as VBUS detection, which also could wake up the chip from all low power mode (includes LLS mode or VLLSx mode (using LLWU module with external pin)).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The VBUS connects to VREGIN and a GPIO pin doesn't cause conflict. I think customer can fly a wise to connect VBUS with related GPIO pin.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this information helps you&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jan 2017 21:06:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-K21-USBDCD-use-for-detect-VBUS-status/m-p/630145#M37912</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-01-26T21:06:14Z</dc:date>
    </item>
  </channel>
</rss>