<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What is in the Kinetis Bootloader Configuration Area (BCA) at the factory default ? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-in-the-Kinetis-Bootloader-Configuration-Area-BCA-at-the/m-p/629553#M37859</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rysard Suboc,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The KL82 boot source is from ROM in default if you didn't download the code before.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Boot source selection bit is in the FOPT, the flash address is 0X40D.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17601iAFCD4618685019DA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;FOPT default data is 0xff, it means the code is boot from the ROM in default.&lt;/P&gt;&lt;P&gt;About the BCA, it is in default all 0xff, it means the KL82 already enable all the perpherals(LPUART, I2C, SPI and USB).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Apr 2017 05:54:41 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2017-04-05T05:54:41Z</dc:date>
    <item>
      <title>What is in the Kinetis Bootloader Configuration Area (BCA) at the factory default ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-in-the-Kinetis-Bootloader-Configuration-Area-BCA-at-the/m-p/629552#M37858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need enter to KL82Z bootloader with&amp;nbsp;BOOTCFG0 and NMI pin assertation.&amp;nbsp;&lt;BR /&gt;When I used bootloader configuration file &lt;EM&gt;system_MKL82Z7.c&amp;nbsp;&lt;/EM&gt;and download code to board and try enter to bootloader with NMI pin, it succeeds.&lt;BR /&gt;&lt;BR /&gt;How enter to bootloader without using bootloader configuration file, when chip is new (from factory), without code?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Mar 2017 10:15:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-in-the-Kinetis-Bootloader-Configuration-Area-BCA-at-the/m-p/629552#M37858</guid>
      <dc:creator>rysardsuboc</dc:creator>
      <dc:date>2017-03-29T10:15:13Z</dc:date>
    </item>
    <item>
      <title>Re: What is in the Kinetis Bootloader Configuration Area (BCA) at the factory default ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-in-the-Kinetis-Bootloader-Configuration-Area-BCA-at-the/m-p/629553#M37859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rysard Suboc,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The KL82 boot source is from ROM in default if you didn't download the code before.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Boot source selection bit is in the FOPT, the flash address is 0X40D.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17601iAFCD4618685019DA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;FOPT default data is 0xff, it means the code is boot from the ROM in default.&lt;/P&gt;&lt;P&gt;About the BCA, it is in default all 0xff, it means the KL82 already enable all the perpherals(LPUART, I2C, SPI and USB).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Apr 2017 05:54:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-in-the-Kinetis-Bootloader-Configuration-Area-BCA-at-the/m-p/629553#M37859</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-04-05T05:54:41Z</dc:date>
    </item>
  </channel>
</rss>