<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 KV30 Input Protection</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV30-Input-Protection/m-p/628406#M37752</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The datasheet for the KV30 implies that inputs are protected from a positive overvoltage&amp;nbsp;if a current limiting resistor is used:&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="JA"&gt;"All analog and I/O pins are internally clamped to V&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;SS &lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;through ESD protection diodes. If V&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;IN &lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;is less than V&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;IO_MIN &lt;/SPAN&gt;&lt;STRONG&gt;&lt;SPAN lang="JA"&gt;or&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;greater than V&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;IO_MAX&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;, a current limiting resistor is required. The negative DC injection current limiting resistor is&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;calculated as R=(V&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;IO_MIN&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;-V&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;IN&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;)/|I&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;ICIO&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;|."&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;However testing this with a 100k input resistor, the device does not seem to clamp the input voltage (tested up to 6.5 V which is well in excess of the 'VIO_MAX').&amp;nbsp; This makes sense since the datasheet also says that pins are only clamped to VSS, so I am wondering if the inputs are actually protected from overvoltage events like implied.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Oct 2016 13:00:57 GMT</pubDate>
    <dc:creator>dillonkopecky</dc:creator>
    <dc:date>2016-10-12T13:00:57Z</dc:date>
    <item>
      <title>KV30 Input Protection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV30-Input-Protection/m-p/628406#M37752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The datasheet for the KV30 implies that inputs are protected from a positive overvoltage&amp;nbsp;if a current limiting resistor is used:&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="JA"&gt;"All analog and I/O pins are internally clamped to V&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;SS &lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;through ESD protection diodes. If V&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;IN &lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;is less than V&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;IO_MIN &lt;/SPAN&gt;&lt;STRONG&gt;&lt;SPAN lang="JA"&gt;or&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;greater than V&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;IO_MAX&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;, a current limiting resistor is required. The negative DC injection current limiting resistor is&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;calculated as R=(V&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;IO_MIN&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;-V&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;IN&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;)/|I&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;ICIO&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;|."&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;However testing this with a 100k input resistor, the device does not seem to clamp the input voltage (tested up to 6.5 V which is well in excess of the 'VIO_MAX').&amp;nbsp; This makes sense since the datasheet also says that pins are only clamped to VSS, so I am wondering if the inputs are actually protected from overvoltage events like implied.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="JA"&gt;&lt;SPAN lang="JA"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 13:00:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV30-Input-Protection/m-p/628406#M37752</guid>
      <dc:creator>dillonkopecky</dc:creator>
      <dc:date>2016-10-12T13:00:57Z</dc:date>
    </item>
    <item>
      <title>Re: KV30 Input Protection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV30-Input-Protection/m-p/628407#M37753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a similar thread about input voltage positive overvoltage requirement and protection circuit with below link:&lt;BR /&gt;&lt;A class="jive-link-thread-small" data-containerid="2019" data-containertype="14" data-objectid="433880" data-objecttype="1" href="https://community.nxp.com/thread/433880"&gt;https://community.nxp.com/thread/433880&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The input voltage should not exceed with datasheet requirement a max. value 3.8V.&lt;BR /&gt;There requires an external diode to VDD, Injected current must be limited to prevent disruption to the internal supply rails.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3948iF98464AD66321335/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Oct 2016 03:18:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV30-Input-Protection/m-p/628407#M37753</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-10-17T03:18:07Z</dc:date>
    </item>
  </channel>
</rss>