<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックCode for 1ms withTMR module</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-for-1ms-withTMR-module/m-p/627938#M37706</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have to generate delay for my MICRO S32KXXX for 1 ms second.&lt;/P&gt;&lt;P&gt;I have gone through number of post, which are related to LPTMR module to generate delay for application .&lt;/P&gt;&lt;P&gt;I also followed up the LPTMR module in K60P144M micro and tried here to write the code for generation dealy for 1 ms.&lt;/P&gt;&lt;P&gt;I want to use OSC0ERCLK clock for LPTMR module, my crystal is of 8 MHz.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 17 Sep 2016 15:16:35 GMT</pubDate>
    <dc:creator>yashkumar</dc:creator>
    <dc:date>2016-09-17T15:16:35Z</dc:date>
    <item>
      <title>Code for 1ms withTMR module</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-for-1ms-withTMR-module/m-p/627938#M37706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have to generate delay for my MICRO S32KXXX for 1 ms second.&lt;/P&gt;&lt;P&gt;I have gone through number of post, which are related to LPTMR module to generate delay for application .&lt;/P&gt;&lt;P&gt;I also followed up the LPTMR module in K60P144M micro and tried here to write the code for generation dealy for 1 ms.&lt;/P&gt;&lt;P&gt;I want to use OSC0ERCLK clock for LPTMR module, my crystal is of 8 MHz.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Sep 2016 15:16:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-for-1ms-withTMR-module/m-p/627938#M37706</guid>
      <dc:creator>yashkumar</dc:creator>
      <dc:date>2016-09-17T15:16:35Z</dc:date>
    </item>
    <item>
      <title>Re: Code for 1ms with LPTMR module</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-for-1ms-withTMR-module/m-p/627939#M37707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the same question from below thread:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/434930"&gt;https://community.nxp.com/thread/434930&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Sep 2016 02:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-for-1ms-withTMR-module/m-p/627939#M37707</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-09-19T02:22:25Z</dc:date>
    </item>
  </channel>
</rss>