<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic  32 bit bus in multiplexed mode in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/32-bit-bus-in-multiplexed-mode/m-p/627507#M37683</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am using TWR-K60F120M tower , I want to configure 32 bit bus in multiplexed mode. Please suggest the Register &amp;nbsp; configuration (The board is working fine in 16 bit non multiplexed mode).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Nov 2016 07:11:38 GMT</pubDate>
    <dc:creator>immanuelraja</dc:creator>
    <dc:date>2016-11-03T07:11:38Z</dc:date>
    <item>
      <title>32 bit bus in multiplexed mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/32-bit-bus-in-multiplexed-mode/m-p/627507#M37683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am using TWR-K60F120M tower , I want to configure 32 bit bus in multiplexed mode. Please suggest the Register &amp;nbsp; configuration (The board is working fine in 16 bit non multiplexed mode).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Nov 2016 07:11:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/32-bit-bus-in-multiplexed-mode/m-p/627507#M37683</guid>
      <dc:creator>immanuelraja</dc:creator>
      <dc:date>2016-11-03T07:11:38Z</dc:date>
    </item>
    <item>
      <title>Re:  32 bit bus in multiplexed mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/32-bit-bus-in-multiplexed-mode/m-p/627508#M37684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Immanuel,&lt;/P&gt;&lt;P&gt;If you use 32 bits multiplexed mode, from hardware perspective, you have to use 32 bits latch device to latch the address in the address stage of FlexBus timing.&lt;/P&gt;&lt;P&gt;From software perspective, you have to set the port size bits FB_CSCRn[ps]=00 in binary, and set the&amp;nbsp;FB_CSPMCR register if you use byte enbale signals.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Feb 2017 08:01:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/32-bit-bus-in-multiplexed-mode/m-p/627508#M37684</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-02-16T08:01:32Z</dc:date>
    </item>
  </channel>
</rss>