<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Problem connection with ethernet port use 3.3V external power supply</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-connection-with-ethernet-port-use-3-3V-external-power/m-p/626330#M37568</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hola Hui_Ma&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #666666; font-size: 14px; margin: 0px 0px 1.7rem; padding: 0px;"&gt;I designed the hardware around the FRDM-K64F. But this is simple, it consists of a power source of 3.3v @ 100mA. In addition to analog / digital inputs / outputs.&amp;nbsp;&lt;SPAN&gt; I energized the K64F through the pins 4 and 6 of the J3 (P3V3). Is this advisable? Or it is best to do it through the pin 16 (J3) 5_9V or J24 connector?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #666666; font-size: 14px; margin: 0px 0px 1.7rem; padding: 0px;"&gt;The problem is after the K64 is running in continuous mode. If there is a power outage when resetting in the short time (10 sec), it does not connect the K64's ethernet port to the network.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Jan 2017 14:17:08 GMT</pubDate>
    <dc:creator>juanolivero</dc:creator>
    <dc:date>2017-01-19T14:17:08Z</dc:date>
    <item>
      <title>Problem connection with ethernet port use 3.3V external power supply</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-connection-with-ethernet-port-use-3-3V-external-power/m-p/626328#M37566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;BR /&gt;I need help with the following problem.&lt;BR /&gt;I am using an FRDM-K64F powered with an external 3.3V source.&lt;BR /&gt;When connecting ethernet port to pc, sometimes does not connect pc with K64F. After restarting the external source several times connect.&lt;BR /&gt;I can not find the reason. Can it be bad configuration of the ethernet port of the K64F? Problem in the transient current of the external source?&lt;BR /&gt;Thank you. Greetings.&lt;BR /&gt;Juan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 00:19:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-connection-with-ethernet-port-use-3-3V-external-power/m-p/626328#M37566</guid>
      <dc:creator>juanolivero</dc:creator>
      <dc:date>2017-01-19T00:19:20Z</dc:date>
    </item>
    <item>
      <title>Re: Problem connection with ethernet port use 3.3V external power supply</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-connection-with-ethernet-port-use-3-3V-external-power/m-p/626329#M37567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If customer using J24 provided power to FRDM-K64F board? Please check the power source driver capability.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11614iB258A6065F5E024F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 05:44:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-connection-with-ethernet-port-use-3-3V-external-power/m-p/626329#M37567</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-01-19T05:44:18Z</dc:date>
    </item>
    <item>
      <title>Re: Problem connection with ethernet port use 3.3V external power supply</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-connection-with-ethernet-port-use-3-3V-external-power/m-p/626330#M37568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hola Hui_Ma&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #666666; font-size: 14px; margin: 0px 0px 1.7rem; padding: 0px;"&gt;I designed the hardware around the FRDM-K64F. But this is simple, it consists of a power source of 3.3v @ 100mA. In addition to analog / digital inputs / outputs.&amp;nbsp;&lt;SPAN&gt; I energized the K64F through the pins 4 and 6 of the J3 (P3V3). Is this advisable? Or it is best to do it through the pin 16 (J3) 5_9V or J24 connector?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #666666; font-size: 14px; margin: 0px 0px 1.7rem; padding: 0px;"&gt;The problem is after the K64 is running in continuous mode. If there is a power outage when resetting in the short time (10 sec), it does not connect the K64's ethernet port to the network.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 14:17:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-connection-with-ethernet-port-use-3-3V-external-power/m-p/626330#M37568</guid>
      <dc:creator>juanolivero</dc:creator>
      <dc:date>2017-01-19T14:17:08Z</dc:date>
    </item>
    <item>
      <title>Re: Problem connection with ethernet port use 3.3V external power supply</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-connection-with-ethernet-port-use-3-3V-external-power/m-p/626331#M37569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We prefer to add the voltage at J24 or&amp;nbsp;&lt;SPAN&gt;pin 16 (J3) 5_9V&lt;/SPAN&gt; with FRDM-K64F U17 NCP1117ST33T3G regulator, which provides the K64 3.3V voltage.&lt;/P&gt;&lt;P&gt;While, from the NCP1117ST33T3G regulator datasheet, the VIN voltage should be in range of [4.75V to 10V].&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12819i00E52B1CA8CC9993/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 22 Jan 2017 05:51:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-connection-with-ethernet-port-use-3-3V-external-power/m-p/626331#M37569</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-01-22T05:51:36Z</dc:date>
    </item>
  </channel>
</rss>