<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: uart pass-through KL17</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/uart-pass-through-KL17/m-p/626065#M37543</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can get UART&amp;lt;-&amp;gt;LPUART DMA or interrupt based pass-through in the uTasker project (works for m0+ and m4 based Kinetis processors).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, it can do pass-through without the need for UART by transferring GPIOs from one pin to another based on port change triggered DMA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Nov 2016 22:40:31 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2016-11-25T22:40:31Z</dc:date>
    <item>
      <title>uart pass-through KL17</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/uart-pass-through-KL17/m-p/626064#M37542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to implement an uart pass-through using two ports: uart2 and lpuart0 on the Kinetis KL17. (using KD1.3)&lt;BR /&gt;To implement this pass-through I would like to use DMA. I have tried implementing it, but so far I could not make it work.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My code setup is attached.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help is appreciated.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;TIA.&lt;/P&gt;&lt;P&gt;-rd&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337445"&gt;dma_init.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2016 21:04:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/uart-pass-through-KL17/m-p/626064#M37542</guid>
      <dc:creator>renatodutra</dc:creator>
      <dc:date>2016-11-25T21:04:56Z</dc:date>
    </item>
    <item>
      <title>Re: uart pass-through KL17</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/uart-pass-through-KL17/m-p/626065#M37543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can get UART&amp;lt;-&amp;gt;LPUART DMA or interrupt based pass-through in the uTasker project (works for m0+ and m4 based Kinetis processors).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, it can do pass-through without the need for UART by transferring GPIOs from one pin to another based on port change triggered DMA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2016 22:40:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/uart-pass-through-KL17/m-p/626065#M37543</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-11-25T22:40:31Z</dc:date>
    </item>
    <item>
      <title>Re: uart pass-through KL17</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/uart-pass-through-KL17/m-p/626066#M37544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the suggestion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At this point not planning to add "middleware" to the project, however this may be explored in the future.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;-rd&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Nov 2016 18:21:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/uart-pass-through-KL17/m-p/626066#M37544</guid>
      <dc:creator>renatodutra</dc:creator>
      <dc:date>2016-11-28T18:21:17Z</dc:date>
    </item>
    <item>
      <title>Re: uart pass-through KL17</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/uart-pass-through-KL17/m-p/626067#M37545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi renatodutra,&lt;/P&gt;&lt;P&gt;Have you try to use the dma_transfer examples in SDK_2.1_MKL17Z256xxx4?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9424iEE88D7EFC6F9F4B9/image-size/large?v=v2&amp;amp;px=999" title="dma_transfer lpuart uart.png" alt="dma_transfer lpuart uart.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The newer version KSDK is recommanded to use. You can build and download the SDK_2.1_MKL17Z256xxx4 from &lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fmcuxpresso.nxp.com%2Fen%2Fwelcome" rel="nofollow" target="_blank"&gt;MCUXpresso Config Tools&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;---------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Nov 2016 09:15:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/uart-pass-through-KL17/m-p/626067#M37545</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2016-11-29T09:15:50Z</dc:date>
    </item>
  </channel>
</rss>