<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KwikStik working with SD card in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KwikStik-working-with-SD-card/m-p/215947#M3740</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For those who want to use a SD card with kwikStik we are pleased to announce our very first emulated SPI driver for SD card. We emulate the SPI pins trough IOs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now it is possible to access the SD card of the KwikStik kit. It is not so fast, but works.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Source code can be download here. We only tested it written into the FLASH (not in RAM).&lt;/P&gt;&lt;P&gt;&lt;A href="http://brtos.googlecode.com/files/BRTOS%201.6x%20K40%20-%20SD%20card.rar" rel="nofollow" target="_blank"&gt;http://brtos.googlecode.com/files/BRTOS%201.6x%20K40%20-%20SD%20card.rar&lt;/A&gt;﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gustavo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 18 Jun 2011 03:27:45 GMT</pubDate>
    <dc:creator>gustavod</dc:creator>
    <dc:date>2011-06-18T03:27:45Z</dc:date>
    <item>
      <title>KwikStik working with SD card</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KwikStik-working-with-SD-card/m-p/215947#M3740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For those who want to use a SD card with kwikStik we are pleased to announce our very first emulated SPI driver for SD card. We emulate the SPI pins trough IOs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now it is possible to access the SD card of the KwikStik kit. It is not so fast, but works.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Source code can be download here. We only tested it written into the FLASH (not in RAM).&lt;/P&gt;&lt;P&gt;&lt;A href="http://brtos.googlecode.com/files/BRTOS%201.6x%20K40%20-%20SD%20card.rar" rel="nofollow" target="_blank"&gt;http://brtos.googlecode.com/files/BRTOS%201.6x%20K40%20-%20SD%20card.rar&lt;/A&gt;﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gustavo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Jun 2011 03:27:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KwikStik-working-with-SD-card/m-p/215947#M3740</guid>
      <dc:creator>gustavod</dc:creator>
      <dc:date>2011-06-18T03:27:45Z</dc:date>
    </item>
    <item>
      <title>Re: KwikStik working with SD card</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KwikStik-working-with-SD-card/m-p/215948#M3741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kwikstik has test pads for SD card connector pins.&lt;/P&gt;&lt;P&gt;And unconnected SDHC0_D0~D3 are all connected to TWRPI or PCI connectors.&lt;/P&gt;&lt;P&gt;So I think we can enable SD card mode access by solder the test pads to that connector pins and set wrongly connected D4~D6 as input...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jun 2011 17:01:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KwikStik-working-with-SD-card/m-p/215948#M3741</guid>
      <dc:creator>Dekiru</dc:creator>
      <dc:date>2011-06-29T17:01:14Z</dc:date>
    </item>
  </channel>
</rss>