<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Kinetis MK70</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK70/m-p/215806#M3737</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I developed a project with Kinetis PK70 to 120MHz.&lt;/P&gt;&lt;P&gt;I'm going through the production with the Kinetis MK70 up to 150MHz.&lt;/P&gt;&lt;P&gt;Wondering if the firmware developed with CodeWarrior 10.3 and MQX 3.8, are compatible or need to change the setting to run MK70.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maurizio&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Dec 2012 15:23:27 GMT</pubDate>
    <dc:creator>Microfelix</dc:creator>
    <dc:date>2012-12-21T15:23:27Z</dc:date>
    <item>
      <title>Kinetis MK70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK70/m-p/215806#M3737</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I developed a project with Kinetis PK70 to 120MHz.&lt;/P&gt;&lt;P&gt;I'm going through the production with the Kinetis MK70 up to 150MHz.&lt;/P&gt;&lt;P&gt;Wondering if the firmware developed with CodeWarrior 10.3 and MQX 3.8, are compatible or need to change the setting to run MK70.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maurizio&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Dec 2012 15:23:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK70/m-p/215806#M3737</guid>
      <dc:creator>Microfelix</dc:creator>
      <dc:date>2012-12-21T15:23:27Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK70/m-p/215807#M3738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maurizio, most likely you would have to change a couple of register settings in the MCG module, aside from that your code does not need to have any changes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2013 17:09:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK70/m-p/215807#M3738</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2013-01-09T17:09:21Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK70/m-p/215808#M3739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there a new BSP for the MK70 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;have the same problem .. we are using the MQX ..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 May 2013 14:35:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK70/m-p/215808#M3739</guid>
      <dc:creator>monXii</dc:creator>
      <dc:date>2013-05-02T14:35:08Z</dc:date>
    </item>
  </channel>
</rss>