<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: VREF vs bandgap voltage reference (aka system reference voltage)</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VREF-vs-bandgap-voltage-reference-aka-system-reference-voltage/m-p/622190#M37264</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Internal bandgap cannot be internally selected as any 'direct' ADC reference --- you CAN 'promptly' convert the bandgap alongside your analog-of-interest and 'calculate back' the 'true' value of Vref at the moment, BUT note that the Kinetis internal bandgaps are only rated +/-3% (as noted in the datasheet Vbg), and even a good NCP1117 (or similar 2% part) Vdd regulator would be better than that, without this extra step!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jan 2017 15:11:57 GMT</pubDate>
    <dc:creator>egoodii</dc:creator>
    <dc:date>2017-01-17T15:11:57Z</dc:date>
    <item>
      <title>VREF vs bandgap voltage reference (aka system reference voltage)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VREF-vs-bandgap-voltage-reference-aka-system-reference-voltage/m-p/622188#M37262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On a processors such as the KL27 family, either the bandgap voltage reference or &amp;nbsp;VREF can be used as reference inputs to the ADC. &amp;nbsp;This leads to two questions:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Since VREF is actually derived from the bandgap voltage reference, when (and why) would you use VREF as a reference input rather than the bandgap voltage reference?&lt;/LI&gt;&lt;LI&gt;What is the bandgap voltage? &amp;nbsp;Some documents suggest that it is 1.0 V, other documents suggest that it's 1.2V. &amp;nbsp;(I guess the real question is: where do I find the electrical specifications for the KL27 family of processors, in particular Vbe?)&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jan 2017 21:11:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/VREF-vs-bandgap-voltage-reference-aka-system-reference-voltage/m-p/622188#M37262</guid>
      <dc:creator>robertpoor</dc:creator>
      <dc:date>2017-01-16T21:11:12Z</dc:date>
    </item>
    <item>
      <title>Re: VREF vs bandgap voltage reference (aka system reference voltage)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VREF-vs-bandgap-voltage-reference-aka-system-reference-voltage/m-p/622189#M37263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1&amp;gt; The Bandgap voltage (PMC module provided) could not be used as ADC reference voltage, while VREF module provides VREF_OUT pin could be working as ADC module reference voltage. The ADC module channel 27 listed Bandgap is PMC bandgap 1V reference voltage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2&amp;gt;&amp;nbsp; The PMC bandgap voltage is listed at Table 6 of &lt;A href="http://www.nxp.com/assets/documents/data/en/data-sheets/KL27P64M48SF6.pdf"&gt;KL27 datasheet&lt;/A&gt;:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11493iCC2145D34E7437E1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11537iE1E9E7520E46AE66/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jan 2017 07:06:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/VREF-vs-bandgap-voltage-reference-aka-system-reference-voltage/m-p/622189#M37263</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-01-17T07:06:44Z</dc:date>
    </item>
    <item>
      <title>Re: VREF vs bandgap voltage reference (aka system reference voltage)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VREF-vs-bandgap-voltage-reference-aka-system-reference-voltage/m-p/622190#M37264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Internal bandgap cannot be internally selected as any 'direct' ADC reference --- you CAN 'promptly' convert the bandgap alongside your analog-of-interest and 'calculate back' the 'true' value of Vref at the moment, BUT note that the Kinetis internal bandgaps are only rated +/-3% (as noted in the datasheet Vbg), and even a good NCP1117 (or similar 2% part) Vdd regulator would be better than that, without this extra step!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jan 2017 15:11:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/VREF-vs-bandgap-voltage-reference-aka-system-reference-voltage/m-p/622190#M37264</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2017-01-17T15:11:57Z</dc:date>
    </item>
  </channel>
</rss>