<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Please Clarify FSEC with Bootloader</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-Clarify-FSEC-with-Bootloader/m-p/622127#M37258</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kerry:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0x40c set to 0 or 0xff would be no different correct? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You just don't want bits 0 and 1 to be b10 -- then you made a brick. &amp;nbsp;The rest of the byte decides if the key is active, mass erase possible, NXP and read the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Nov 2016 10:42:26 GMT</pubDate>
    <dc:creator>JHinkle</dc:creator>
    <dc:date>2016-11-02T10:42:26Z</dc:date>
    <item>
      <title>Please Clarify FSEC with Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-Clarify-FSEC-with-Bootloader/m-p/622123#M37254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want my KL17 and K64 devices to be secure yet be able to erase them if needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FSEC is read and processed during reset which will make the FSEC associated with the bootloader take precedence.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please clarify my understanding that the FSEC, FPROT, ect setting of the the application code have no bearing on how the device behaves.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Nov 2016 11:44:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-Clarify-FSEC-with-Bootloader/m-p/622123#M37254</guid>
      <dc:creator>JHinkle</dc:creator>
      <dc:date>2016-11-01T11:44:11Z</dc:date>
    </item>
    <item>
      <title>Re: Please Clarify FSEC with Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-Clarify-FSEC-with-Bootloader/m-p/622124#M37255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Only the boot loader can set the Flash configuration parameters. The application never has any such.&lt;/P&gt;&lt;P&gt;It may be that the code "does have a table" but it will be located at an address that is not relevant to the reset and so its of no use.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Nov 2016 19:18:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-Clarify-FSEC-with-Bootloader/m-p/622124#M37255</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-11-01T19:18:41Z</dc:date>
    </item>
    <item>
      <title>Re: Please Clarify FSEC with Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-Clarify-FSEC-with-Bootloader/m-p/622125#M37256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the confirmation Mark.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That's what I thought - just wanted to confirm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Nov 2016 21:16:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-Clarify-FSEC-with-Bootloader/m-p/622125#M37256</guid>
      <dc:creator>JHinkle</dc:creator>
      <dc:date>2016-11-01T21:16:33Z</dc:date>
    </item>
    <item>
      <title>Re: Please Clarify FSEC with Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-Clarify-FSEC-with-Bootloader/m-p/622126#M37257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joe,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The most important data is the Flash configuration filed:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6255i68C806D9741F9D15/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The flash configuration field is in the bootloader area, so you don't need to afraid that the APP will modify it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Just make sure the 0X40D, 0X40C data is which you need, if you want to secure and enable the erase,&amp;nbsp; don't protect the area which you want to erase, and set 0X40C data to 0x03.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please contact me!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Nov 2016 08:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-Clarify-FSEC-with-Bootloader/m-p/622126#M37257</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-11-02T08:52:06Z</dc:date>
    </item>
    <item>
      <title>Re: Please Clarify FSEC with Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-Clarify-FSEC-with-Bootloader/m-p/622127#M37258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kerry:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0x40c set to 0 or 0xff would be no different correct? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You just don't want bits 0 and 1 to be b10 -- then you made a brick. &amp;nbsp;The rest of the byte decides if the key is active, mass erase possible, NXP and read the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Nov 2016 10:42:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-Clarify-FSEC-with-Bootloader/m-p/622127#M37258</guid>
      <dc:creator>JHinkle</dc:creator>
      <dc:date>2016-11-02T10:42:26Z</dc:date>
    </item>
    <item>
      <title>Re: Please Clarify FSEC with Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-Clarify-FSEC-with-Bootloader/m-p/622128#M37259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joe,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The detail meaning of 0X40C data is in the FTFE_FSEC register:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6691i3E0E85BE55562AED/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; So, the data 0x00 or 0XFF in address 0x40c is the same, if you want to secure the chip, just make sure SEC bit is not unsecured(0b10).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please contact me!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Nov 2016 02:25:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-Clarify-FSEC-with-Bootloader/m-p/622128#M37259</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-11-03T02:25:50Z</dc:date>
    </item>
  </channel>
</rss>