<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Is brownout detection available in MKL17Z64VFM4</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-brownout-detection-available-in-MKL17Z64VFM4/m-p/621902#M37219</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes,Is it possible to configure the LVD with user defined value.I want to detect power failure &amp;nbsp;when chip voltage is less than 2.8V is it possible.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Sep 2016 13:34:32 GMT</pubDate>
    <dc:creator>jagadeeshkumar</dc:creator>
    <dc:date>2016-09-16T13:34:32Z</dc:date>
    <item>
      <title>Is brownout detection available in MKL17Z64VFM4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-brownout-detection-available-in-MKL17Z64VFM4/m-p/621900#M37217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;I was looking at the data sheets there they mentioned no brown out is it is available or not.Could any one suggest me please.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Sep 2016 12:32:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-brownout-detection-available-in-MKL17Z64VFM4/m-p/621900#M37217</guid>
      <dc:creator>jagadeeshkumar</dc:creator>
      <dc:date>2016-09-15T12:32:08Z</dc:date>
    </item>
    <item>
      <title>Re: Is brownout detection available in MKL17Z64VFM4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-brownout-detection-available-in-MKL17Z64VFM4/m-p/621901#M37218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is "Low Voltage Detect" in the Power Management Controller what you are looking for?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Sep 2016 12:11:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-brownout-detection-available-in-MKL17Z64VFM4/m-p/621901#M37218</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2016-09-16T12:11:31Z</dc:date>
    </item>
    <item>
      <title>Re: Is brownout detection available in MKL17Z64VFM4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-brownout-detection-available-in-MKL17Z64VFM4/m-p/621902#M37219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes,Is it possible to configure the LVD with user defined value.I want to detect power failure &amp;nbsp;when chip voltage is less than 2.8V is it possible.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Sep 2016 13:34:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-brownout-detection-available-in-MKL17Z64VFM4/m-p/621902#M37219</guid>
      <dc:creator>jagadeeshkumar</dc:creator>
      <dc:date>2016-09-16T13:34:32Z</dc:date>
    </item>
    <item>
      <title>Re: Is brownout detection available in MKL17Z64VFM4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-brownout-detection-available-in-MKL17Z64VFM4/m-p/621903#M37220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jagadeesh Kumar&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can not configure LVD with user defined value, but you can select the voltage detect:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5183iB753A6741D3DDCA2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;where:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5224i94FAA2F888AD23C2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alternately you can use the "low voltage warning function" in the same module. I recommend you to check the chapter 15 of the Reference manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information helps you.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Sep 2016 19:44:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-brownout-detection-available-in-MKL17Z64VFM4/m-p/621903#M37220</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2016-09-17T19:44:30Z</dc:date>
    </item>
    <item>
      <title>Re: Is brownout detection available in MKL17Z64VFM4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-brownout-detection-available-in-MKL17Z64VFM4/m-p/621904#M37221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bits in the Reset Control Module will say if the reset is due to a power up:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*lint -save -e514 */&lt;BR /&gt; rst_b |= (0U != (RCM_SSRS0 &amp;amp; (RCM_SSRS0_SPOR_MASK|RCM_SSRS0_SLVD_MASK))); /* Return not zero when Power On Reset or Low Voltage Detect bits are set */&lt;BR /&gt; /*lint -restore */&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Sep 2016 14:29:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-brownout-detection-available-in-MKL17Z64VFM4/m-p/621904#M37221</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2016-09-19T14:29:32Z</dc:date>
    </item>
  </channel>
</rss>