<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Analogue reference voltage pin in MKL03Z8VFG4</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Analogue-reference-voltage-pin-in-MKL03Z8VFG4/m-p/621529#M37191</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;Thanks for the reply. The reference manual solves the purpose. It mentions how to use the internal 1.2V source as VREF for the ADC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mrinal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Mar 2017 08:43:37 GMT</pubDate>
    <dc:creator>mrinal</dc:creator>
    <dc:date>2017-03-09T08:43:37Z</dc:date>
    <item>
      <title>Analogue reference voltage pin in MKL03Z8VFG4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Analogue-reference-voltage-pin-in-MKL03Z8VFG4/m-p/621527#M37189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;My application requires sampling of three analogue lines and transmitting the results via serial line.&lt;/P&gt;&lt;P&gt;I am thinking to use&amp;nbsp;MKL03Z8VFG4.&lt;/P&gt;&lt;P&gt;But I am not sure about the analogue reference voltage pin. The datasheet says (on page number 34): &amp;nbsp;"For packages without dedicated VREFH and VREFL pins, VREFH is internally tied to VDDA, and VREFL is internally tied to VSSA".&lt;/P&gt;&lt;P&gt;The 16-pin package does not have&amp;nbsp;dedicated VREFH and VREFL. So the reference pin should be internally tied to VDDA. However the package does not even have a VDDA pin. As far as power is concerned, there are only two pins i.e. VDD and VSS.&lt;/P&gt;&lt;P&gt;What does this mean? Does it mean that VDDA and VDD are the same? The datasheet also mentions that there is a &amp;nbsp;1.2V on chip voltage reference. How to use this reference?&lt;/P&gt;&lt;P&gt;Please help...&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Mar 2017 12:27:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Analogue-reference-voltage-pin-in-MKL03Z8VFG4/m-p/621527#M37189</guid>
      <dc:creator>mrinal</dc:creator>
      <dc:date>2017-03-04T12:27:42Z</dc:date>
    </item>
    <item>
      <title>Re: Analogue reference voltage pin in MKL03Z8VFG4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Analogue-reference-voltage-pin-in-MKL03Z8VFG4/m-p/621528#M37190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mrinal Mani,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1. Analog reference pin&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/16417i37D39898BC704EE6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/16464i92E1924AB0E95AD4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So, VREFH, VDD, VDDA is the same pin in VDD pin. VREFL, VSSA, VSS is the same pin in VSS.&lt;/P&gt;&lt;P&gt;2.&amp;nbsp; 1.2v on chip voltage refernce&lt;/P&gt;&lt;P&gt;VREF_OUT is in pin PTB2, it can output 1.2V.&lt;/P&gt;&lt;P&gt;&amp;nbsp;More details, please refer to the KL02 reference manual, Chapter 30 Voltage Reference (VREF)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please let me know~!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Kerry&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Mar 2017 10:36:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Analogue-reference-voltage-pin-in-MKL03Z8VFG4/m-p/621528#M37190</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-03-06T10:36:56Z</dc:date>
    </item>
    <item>
      <title>Re: Analogue reference voltage pin in MKL03Z8VFG4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Analogue-reference-voltage-pin-in-MKL03Z8VFG4/m-p/621529#M37191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;Thanks for the reply. The reference manual solves the purpose. It mentions how to use the internal 1.2V source as VREF for the ADC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mrinal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 08:43:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Analogue-reference-voltage-pin-in-MKL03Z8VFG4/m-p/621529#M37191</guid>
      <dc:creator>mrinal</dc:creator>
      <dc:date>2017-03-09T08:43:37Z</dc:date>
    </item>
  </channel>
</rss>