<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: multi device on same spi bus</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/multi-device-on-same-spi-bus/m-p/621002#M37159</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bilge kaan ugur,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The PE module just have one CS to select, if you want to add other CS, don't worry, just select one CS at first, but don't use it in the detail code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can use the GPIO used as the according slave CS, before you want to send the data, use code set the according pin as low, after the SPI data is sent, then pull the CS pin high.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please let me know!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Dec 2016 08:32:03 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2016-12-19T08:32:03Z</dc:date>
    <item>
      <title>multi device on same spi bus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/multi-device-on-same-spi-bus/m-p/621001#M37158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying &amp;nbsp;the use SPImaster_LDD component of &amp;nbsp;PE .Cpu is &amp;nbsp;mke04z128 (SPI0). there are more than one slave device on bus. PE &amp;nbsp;does not allow to select cs pin other than pins marked spi0_pcs. &amp;nbsp; how to select more than one cs pin ? &amp;nbsp;I want to use gio pins for cs. what is correct &amp;nbsp;method?&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Dec 2016 22:16:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/multi-device-on-same-spi-bus/m-p/621001#M37158</guid>
      <dc:creator>bilgekaanugur</dc:creator>
      <dc:date>2016-12-18T22:16:31Z</dc:date>
    </item>
    <item>
      <title>Re: multi device on same spi bus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/multi-device-on-same-spi-bus/m-p/621002#M37159</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bilge kaan ugur,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The PE module just have one CS to select, if you want to add other CS, don't worry, just select one CS at first, but don't use it in the detail code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can use the GPIO used as the according slave CS, before you want to send the data, use code set the according pin as low, after the SPI data is sent, then pull the CS pin high.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please let me know!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Dec 2016 08:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/multi-device-on-same-spi-bus/m-p/621002#M37159</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-12-19T08:32:03Z</dc:date>
    </item>
  </channel>
</rss>