<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CAN 2.0 vs SAE J1939 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-2-0-vs-SAE-J1939/m-p/619470#M37006</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The short answer is 'yes', these CAN 2.0 peripherals are EXACTLY what you need for J1939.&amp;nbsp; The way J1939 uses the full-size CAN 2.0 ID just means you have to run the receiver in 'promiscuous mode' and do all traffic filtering in firmware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The longer answer is 'go to Simma Software' for a full high-performance J1939 stack, already guaranteed to run on that uP.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Nov 2016 00:59:12 GMT</pubDate>
    <dc:creator>egoodii</dc:creator>
    <dc:date>2016-11-03T00:59:12Z</dc:date>
    <item>
      <title>CAN 2.0 vs SAE J1939</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-2-0-vs-SAE-J1939/m-p/619469#M37005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using S12 to implement the CAN communication protocol. We would mainly use CAN 2.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the datasheet, It mentions that S12 can support CAN 2.0. May I know can S12 support SAE J1939? As I know CAN 2.0 and SAE J1939 has the similar extended header frame. Are they compatible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Nov 2016 02:51:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-2-0-vs-SAE-J1939/m-p/619469#M37005</guid>
      <dc:creator>monstor</dc:creator>
      <dc:date>2016-11-01T02:51:22Z</dc:date>
    </item>
    <item>
      <title>Re: CAN 2.0 vs SAE J1939</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-2-0-vs-SAE-J1939/m-p/619470#M37006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The short answer is 'yes', these CAN 2.0 peripherals are EXACTLY what you need for J1939.&amp;nbsp; The way J1939 uses the full-size CAN 2.0 ID just means you have to run the receiver in 'promiscuous mode' and do all traffic filtering in firmware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The longer answer is 'go to Simma Software' for a full high-performance J1939 stack, already guaranteed to run on that uP.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Nov 2016 00:59:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-2-0-vs-SAE-J1939/m-p/619470#M37006</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2016-11-03T00:59:12Z</dc:date>
    </item>
  </channel>
</rss>