<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 MKE02Z16VLC4 XTAL PIN</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE02Z16VLC4-XTAL-PIN/m-p/618843#M36966</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on a very simple project where I am reading inputs on nearly all the pins of the micro controller MKE02Z16VLC4 and sending the data over to serial port.&lt;/P&gt;&lt;P&gt;I am also not using any external clock source and the problem I am having is reading the input from XTAL pin.&lt;/P&gt;&lt;P&gt;I have disabled external crystal oscillator and configured the pin as input like all other pins. However, this pin always report HIGH no matter what i do. What am I missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using KDS and Processor expert.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Anang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Dec 2016 05:53:34 GMT</pubDate>
    <dc:creator>AnangBohra</dc:creator>
    <dc:date>2016-12-16T05:53:34Z</dc:date>
    <item>
      <title>MKE02Z16VLC4 XTAL PIN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE02Z16VLC4-XTAL-PIN/m-p/618843#M36966</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on a very simple project where I am reading inputs on nearly all the pins of the micro controller MKE02Z16VLC4 and sending the data over to serial port.&lt;/P&gt;&lt;P&gt;I am also not using any external clock source and the problem I am having is reading the input from XTAL pin.&lt;/P&gt;&lt;P&gt;I have disabled external crystal oscillator and configured the pin as input like all other pins. However, this pin always report HIGH no matter what i do. What am I missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using KDS and Processor expert.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Anang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Dec 2016 05:53:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE02Z16VLC4-XTAL-PIN/m-p/618843#M36966</guid>
      <dc:creator>AnangBohra</dc:creator>
      <dc:date>2016-12-16T05:53:34Z</dc:date>
    </item>
    <item>
      <title>Re: MKE02Z16VLC4 XTAL PIN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE02Z16VLC4-XTAL-PIN/m-p/618844#M36967</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anang,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have help you create a project based on KDS and PE.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; When I connect PTB6, XTAL pin to GND, the GPIO PDIR according bit(bit 15) =0&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11176iB8E4A7A7D5FC97D1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When I connect PTB6, XTAL pin to 3.3V or 5V, the GPIO PDIR according bit(bit 15) =1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11123i65DCDC6DE9E51326/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, the XTAL pin is working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to my attached code.&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Dec 2016 08:11:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE02Z16VLC4-XTAL-PIN/m-p/618844#M36967</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-12-19T08:11:10Z</dc:date>
    </item>
  </channel>
</rss>