<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Updating FTM_CnV pulls down GPIO</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Updating-FTM-CnV-pulls-down-GPIO/m-p/618811#M36960</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What 'ALT pin function selection' do you have placed for PTA2?&amp;nbsp; It defaults to JTAG/SWO output.&amp;nbsp; I assume this is NOT a 'debug connected' environment...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Sep 2016 18:51:58 GMT</pubDate>
    <dc:creator>egoodii</dc:creator>
    <dc:date>2016-09-14T18:51:58Z</dc:date>
    <item>
      <title>Updating FTM_CnV pulls down GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Updating-FTM-CnV-pulls-down-GPIO/m-p/618810#M36959</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;As I mentioned in the title, I have a bug in my code. Every time that I want to update FTM_CnV register (doesn't matter if 0 or 1 or any number) PTA2 GPIO goes low. I can't find any reason for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any ideas for what may be causing this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Sep 2016 13:20:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Updating-FTM-CnV-pulls-down-GPIO/m-p/618810#M36959</guid>
      <dc:creator>snipex94</dc:creator>
      <dc:date>2016-09-14T13:20:20Z</dc:date>
    </item>
    <item>
      <title>Re: Updating FTM_CnV pulls down GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Updating-FTM-CnV-pulls-down-GPIO/m-p/618811#M36960</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What 'ALT pin function selection' do you have placed for PTA2?&amp;nbsp; It defaults to JTAG/SWO output.&amp;nbsp; I assume this is NOT a 'debug connected' environment...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Sep 2016 18:51:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Updating-FTM-CnV-pulls-down-GPIO/m-p/618811#M36960</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2016-09-14T18:51:58Z</dc:date>
    </item>
    <item>
      <title>Re: Updating FTM_CnV pulls down GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Updating-FTM-CnV-pulls-down-GPIO/m-p/618812#M36961</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is a debug connected environment but the SWD pins are at PTC4 and PTA4 (I don't have a JTAG interface). I forgot to mention that I use&amp;nbsp;S9KEAZN64 mcu. Peripherals connected to PTA2 are KB interrupt, UART0 and I2C0, but I am not using them. I'm only using UART1 if this means anything.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below is a picture from the reference manual for PTA2 pin.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5099i3163F42492846645/image-size/large?v=v2&amp;amp;px=999" title="PTA2 mux.PNG" alt="PTA2 mux.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Update: Since that this issue is not caused by updating FTM_CnV register (it was just my luck that it pulled down the pin at the same time multiple times in a row).&lt;/P&gt;&lt;P&gt;I set a breakpoint at the beginning of the while loop and counted how many times it looped before pulling down the pin.&lt;/P&gt;&lt;P&gt;It was always the same number of times.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This problem is just weird and I would love some help on this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Sep 2016 05:44:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Updating-FTM-CnV-pulls-down-GPIO/m-p/618812#M36961</guid>
      <dc:creator>snipex94</dc:creator>
      <dc:date>2016-09-15T05:44:25Z</dc:date>
    </item>
    <item>
      <title>Re: Updating FTM_CnV pulls down GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Updating-FTM-CnV-pulls-down-GPIO/m-p/618813#M36962</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Kvas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you know that the PTA2 is open drain pin, if you use it in GPIO output mode, an external 5K~10K ohm pull-up resistor is required. Even if you set the PTA2 in input mode, I also suggest you connect an external 5K~10K ohm pull-up resistor.&lt;/P&gt;&lt;P&gt;anyway, pls connect a pull-up resistor and have a try, I suppose what you see is noise if you do not connect pull-up resistor.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Sep 2016 02:47:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Updating-FTM-CnV-pulls-down-GPIO/m-p/618813#M36962</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-09-18T02:47:15Z</dc:date>
    </item>
  </channel>
</rss>