<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollersのトピックare there any differences in the SPI interface block (registers, configuration) of Kinets types MK64FN1M0VLL12, MK64FX512VLL12, MK64FX512VDC12?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/are-there-any-differences-in-the-SPI-interface-block-registers/m-p/618583#M36954</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using MK64FX512VDC12 in the final design.&amp;nbsp;During&amp;nbsp;development I would like to work with the freedom development board with integrated MK64FN1M0VLL12 Controller.&amp;nbsp;Key functionality is the SPI Interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To migrate&amp;nbsp;the SPI-Code from MK64FN1M0VLL12 to&amp;nbsp;MK64FX512VDC12&amp;nbsp;do I have to expect any&amp;nbsp;differences/Troubles?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Apr 2017 12:05:26 GMT</pubDate>
    <dc:creator>martinspichtig</dc:creator>
    <dc:date>2017-04-18T12:05:26Z</dc:date>
    <item>
      <title>are there any differences in the SPI interface block (registers, configuration) of Kinets types MK64FN1M0VLL12, MK64FX512VLL12, MK64FX512VDC12?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/are-there-any-differences-in-the-SPI-interface-block-registers/m-p/618583#M36954</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using MK64FX512VDC12 in the final design.&amp;nbsp;During&amp;nbsp;development I would like to work with the freedom development board with integrated MK64FN1M0VLL12 Controller.&amp;nbsp;Key functionality is the SPI Interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To migrate&amp;nbsp;the SPI-Code from MK64FN1M0VLL12 to&amp;nbsp;MK64FX512VDC12&amp;nbsp;do I have to expect any&amp;nbsp;differences/Troubles?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Apr 2017 12:05:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/are-there-any-differences-in-the-SPI-interface-block-registers/m-p/618583#M36954</guid>
      <dc:creator>martinspichtig</dc:creator>
      <dc:date>2017-04-18T12:05:26Z</dc:date>
    </item>
    <item>
      <title>Re: are there any differences in the SPI interface block (registers, configuration) of Kinets types MK64FN1M0VLL12, MK64FX512VLL12, MK64FX512VDC12?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/are-there-any-differences-in-the-SPI-interface-block-registers/m-p/618584#M36955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin Spichtig&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In terms of SPI module, your three devices use the same SPI module, so in your SPI code it shouldn't be any difference or troubles. I just recommend you to check pinout, MK64FN1M0VLL12 device doesn't have some pins that are available in the MK64FX512VDC12, ones of them are some SPI2 pins:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10030iD9A930224A9CA8F0/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, please consider this if you are using SPI2 interface.&lt;/P&gt;&lt;P&gt;Hope this information could help you.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Apr 2017 00:16:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/are-there-any-differences-in-the-SPI-interface-block-registers/m-p/618584#M36955</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-04-20T00:16:06Z</dc:date>
    </item>
  </channel>
</rss>