<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SWD Debug with MKL26 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SWD-Debug-with-MKL26/m-p/617868#M36857</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Somebody know if need RESET pin to Debug a MKL26 MCU with SWD ??.&lt;/P&gt;&lt;P&gt;I have develop a PCB with QFN MKL26, its a prototype not yet tested, I do not have put the RESET pin to program and Debug the chip, and now Im not sure if I will may Debug it without RESET pin.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have read that some ARM Microcontrollers need RESET, some not. For example recently I tested a ST STM32 and this need RESET pin to do Debug with SWD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Apr 2017 22:08:37 GMT</pubDate>
    <dc:creator>luishs</dc:creator>
    <dc:date>2017-04-17T22:08:37Z</dc:date>
    <item>
      <title>SWD Debug with MKL26</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SWD-Debug-with-MKL26/m-p/617868#M36857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Somebody know if need RESET pin to Debug a MKL26 MCU with SWD ??.&lt;/P&gt;&lt;P&gt;I have develop a PCB with QFN MKL26, its a prototype not yet tested, I do not have put the RESET pin to program and Debug the chip, and now Im not sure if I will may Debug it without RESET pin.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have read that some ARM Microcontrollers need RESET, some not. For example recently I tested a ST STM32 and this need RESET pin to do Debug with SWD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Apr 2017 22:08:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SWD-Debug-with-MKL26/m-p/617868#M36857</guid>
      <dc:creator>luishs</dc:creator>
      <dc:date>2017-04-17T22:08:37Z</dc:date>
    </item>
    <item>
      <title>Re: SWD Debug with MKL26</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SWD-Debug-with-MKL26/m-p/617869#M36858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Luis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just took a look at the &lt;A href="http://www.nxp.com/assets/documents/data/en/reference-manuals/KL26P121M48SF4RM.pdf"&gt;manual&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Seems that your reset is controlled through this register&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12123i46A6572D0536EE09/image-size/large?v=v2&amp;amp;px=999" title="k26debugControlregist.PNG" alt="k26debugControlregist.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Based off of this section here, it seems like you do not need to set it up in software. I would make sure it is properly set up on PCB such that it doesn't float or lock the MCU.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12252iE3BF6FAD6D158E18/image-size/large?v=v2&amp;amp;px=999" title="k26debug.PNG" alt="k26debug.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jason P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Apr 2017 16:16:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SWD-Debug-with-MKL26/m-p/617869#M36858</guid>
      <dc:creator>jasonphilippi</dc:creator>
      <dc:date>2017-04-20T16:16:43Z</dc:date>
    </item>
  </channel>
</rss>